Associate
January 31, 2018
Question
Broken Project from cube v 4.24.0
- January 31, 2018
- 3 replies
- 703 views
Posted on January 31, 2018 at 01:46
so, i've updated cube to v4.24.0
and it starts to make broken .ioc files
i tried several ways to reproduce same issue and here's the problem.
1. make a project with stm32f407ze ( not sure it's because of this but.. )
2. make CAN1 and CAN2 as master mode and slave mode.
3. go to configuration and open up CAN1 setting
4. make Time quanta BS 2 as 7
5. make prescaler to 4
6. make Time quanta BS 1 as 10
7. press okay and save project.
( at this point, you can't open up CAN1 configuration window )
8. and now project is unreadable
my solution to fix this is to manually modify ioc file, removes CAN related configuration