Skip to main content
Amal Babu
Associate III
August 1, 2018
Question

brightness of the led connected to the stm ic pin reduces.

  • August 1, 2018
  • 5 replies
  • 973 views

Hai I have a simple design.I am using STM32F051R4T6TR.I just connected a led such that the led sinks the 20mA current when the led turns on.i happen to notice that each time i switch on my board the brightness of my led is getting reduced.this happened to me many times.The Led turns on with full brightness at first but later on after multiple turn on's the brightness is gradually decreasing and finally thebrightnessis too di, which would ultimately led to changing of the led.What would be the possible reason behind this? Can Anyone suggest me a reason behind this?Will this issue be cleared if i drive an led by sourcing from the pin rather than sinking?

    This topic has been closed for replies.

    5 replies

    T J
    Senior III
    August 1, 2018

    I dont like to drive too hard from the processor pin, it does affect the A/Ds in some configurations,

    however with super bright LEDs, you can get down to 2mA and still see the led easily...

    @20mA I guess the LED is getting hot, it will die one day..

    T J
    Senior III
    August 1, 2018

    best to use a transistor like BC817 then you can drive 100mA..

    Tesla DeLorean
    Guru
    August 1, 2018

    How exactly do you have them wired? Do you have a series resistor to limit current?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Amal Babu
    Amal BabuAuthor
    Associate III
    August 1, 2018

    yes i have placed a series resistance

    T J
    Senior III
    August 1, 2018

    1K ohm is 1mA per volt, less the LED forward voltage drop , 1-2mA... good enough for super brights