Skip to main content
Associate II
November 29, 2023
Solved

breakpoint to breakpoint cycle count ?

hello , where can i see cpu cycle count from one breakpoint to next breakpoint in stmcubeide ? i am using stm32f103 board.

This topic has been closed for replies.
TDK
TDKBest answer
November 30, 2023

There's nothing built-in that will do this.

You can set up a timer that has the same tick rate as the cpu and use that. You'll have to do the math yourself. And you'll have to set the timer so that it's stopped while the chip is paused in debug.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
TDKBest answer
November 30, 2023

There's nothing built-in that will do this.

You can set up a timer that has the same tick rate as the cpu and use that. You'll have to do the math yourself. And you'll have to set the timer so that it's stopped while the chip is paused in debug.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tesla DeLorean
Guru
November 30, 2023

The STM32F1 supports the DWT CYCCNT register, use that to count machine cycles.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate
November 30, 2023

if you want to know the running time between two breakpoint, one suggestion is using a Timer cnt and the other suggestion is to add gpio level change between these breakpoint and use logic analyzer or oscilloscope to measure the time.