Skip to main content
DWWelch
Associate III
September 9, 2025
Question

Both OCTOSPI ports memory mapped on STM32H7A3?

Hello,

I am having trouble memory mapping both OSPI ports at the same time. Can I run a QSPI Flash on OSPI1 and a OSPI Hyperbus RAM on OSPI2 and have both be memory mapped or do both OSPI ports need to be running in the same mode to be memory mapped?

Thanks,

Dan

This topic has been closed for replies.

5 replies

DWWelch
DWWelchAuthor
Associate III
September 9, 2025

I found the issue. If you are using both OSPI ports and use the HAL functions to initialize OSPIManager, when you initialize the second OSPI port with HAL_OSPIM_Config function, it corrupts the OSPIM configuration of the previously initialized OSPI port. I am using STMCubeIDE V1.16 and will try upgrading to V1.18 to see if the issue has been fixed.

Dan

KDJEM.1
ST Technical Moderator
September 9, 2025

Hello @DWWelch ,

 

First of all thank you for sharing this behavior in the community.

Could you please look at this issue Solved: OCTOSPI: HAL_OSPIM_Config() - STMicroelectronics Community. I think you are experiencing the same issue.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
ST Technical Moderator
September 10, 2025

Hello @DWWelch ;

 

To solve the issue could you please try to modify these code lines in octospi.c file

 sOspiManagerCfg.ClkPort = 1;
 sOspiManagerCfg.NCSPort = 1;
 sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;
 if (HAL_OSPIM_Config(&hospi1, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }

 

 sOspiManagerCfg.ClkPort = 2;
 sOspiManagerCfg.NCSPort = 2;
 sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;
 if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }

 

by

 

 sOspiManagerCfg.ClkPort = 1;
 sOspiManagerCfg.NCSPort = 1;
 sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_1_LOW;
 sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_1_HIGH;
 sOspiManagerCfg.DQSPort = 1;
 if (HAL_OSPIM_Config(&hospi1, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }
 

 sOspiManagerCfg.ClkPort = 2;
 sOspiManagerCfg.NCSPort = 2;
 sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;
 sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_2_HIGH;
 sOspiManagerCfg.DQSPort = 2;
 if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
 {
 Error_Handler();
 }

 

Please let me know if the issue is solved or not?

Thank you.

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
DWWelch
DWWelchAuthor
Associate III
September 12, 2025

Hi Kaouthar,

I manually enabled the incorrectly disabled pin functions in the OSPIM->PCR registers and everything works properly. I did not use your method as I do not wish to enable unused OSPI pins that I am using for other functions. They really need to fix this problem. All they need to do is re-enable the OSPI pins of the previously configured port after configuring the second OSPI port pins. The origional pin mapping does not get corrupted, they just become disabled after initializing the second OSPI port.

Thanks,

Dan

KDJEM.1
ST Technical Moderator
October 8, 2025

Hello @DWWelch ,

 

I apologize for any inconvenience.

This is reported internally for more investigation.

Internal ticket number: 203289 (This is an internal tracking number and is not accessible or usable by customers) 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.