Skip to main content
Associate III
Nov 18, 2026 6:25 AM UTC
Question

BOR Level and working voltage of STM32L496

Hi,

We are using STM32L496, BOR level shows,

 

BOR Level 0's falling threshold can be as low as 1.60 V, while the STM32L496 minimum specified operating voltage is 1.71 V.

 

So from 1.71V to 1.60V if its a large enough time, will the MCU functions normally?

 

/Anurag

 

4 replies

waclawek.jan
Super User
Nov 18, 2026 10:30 AM UTC

It’s confusing indeed and a footnote to the BOR thresholds table might be added too. Also, wording of this section might be changed to reflect this:

JW

Associate III
Nov 18, 2026 10:38 AM UTC

Hi, 

Thanks for information.

 

The lowest BOR level is 1.71V at power on  → means → Reset will be released above 1.71V at power on, not 1.62V anyways, right?

waclawek.jan
Super User
Nov 18, 2026 11:18 AM UTC

No.

IMO, in chapter 3.10.2, the “lowest BOR level is 1.71V at power on” is incorrect, and the value from table (1.62V) is correct.

And the footnote to Standard operating voltage means, that while you are not supposed to deliberately design your power supply to be below 1.71V, the mcu will operate correctly at whatever the BOR0 minimum value for that given piece is, if there’s no other source of RESET active.

In other words, this gives you a guarantee that the mcu will operate correctly during VDD powerup ramp as soon as it crosses the minimum rising BOR0 value, and also during VDD powerdown down to minimum falling BOR0 value. Note, that the actual BOR0 levels are dependent on the very details of the semiconductor manufacturing process, that’s why a range is given.

But I am not ST and you may want to wait until somebody from ST comments on this.

JW

mƎALLEm
ST Technical Moderator
Nov 18, 2026 11:44 AM UTC

​@Anuraglokhande ,

Your post have been already escalated to OLS over this ticket number 00273459.

Hope you’ll be served asap.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.