Skip to main content
Associate III
Apr 8, 2025 8:28 AM UTC
Solved

bootloader for STM32G474QET6 - usable UART pins?

I am trying to use the bootloader of the STM32G474QET6 with USART to program my microcontroller. 

I have multiple questions regarding this but the first one is more about hardware. I have found in AN2606 that for the bootloader I can only use one of three USART, as listed under :

EliazLB_0-1744100551282.png

So after this info, I can use either USART1, 2 or 3 but when I look at the pins attached and at the datasheet of my microcontroller, pins for USART3 on the MCU are not PC11 and PC10. 

EliazLB_1-1744100662917.png

The thing is on my PCB I've decided to use PB10 and PB11, and according to the datasheet, they are the pins of USART3.

So my question is pretty simple, which document is right and which should I follow ? Am I going to need to change anything ? 

Thanks for the answers !

This topic has been closed for replies.
Mike_ST
Mike_STBest answer
ST Technical Moderator
Apr 8, 2025 8:53 AM UTC

Hello,

>> pins for USART3 on the MCU are not PC11 and PC10

 

Mike_ST_0-1744102086837.png

 

>> So my question is pretty simple, which document is right and which should I follow ?

Both are right,

>> Am I going to need to change anything

If you want to use the bootloader on USART3, probably you'll need to switch to PC10/PC11.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 

7 replies

Andrew Neil
Super User
Apr 8, 2025 8:49 AM UTC

@EliazLB wrote:

EliazLB_0-1744100551282.png

So after this info, I can use either USART1, 2 or 3 but when I look at the pins attached and at the datasheet of my microcontroller, pins for USART3 on the MCU are not PC11 and PC10.  !


I think what it's telling you is that you can use USART1 on PA9,10; or USART2 on PA2,3; or USART3 on PC10,11.

If your particular chip does not provide those specific pins, then you can't use it on that chip.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Apr 8, 2025 8:52 AM UTC

Hang on!

 


@EliazLB wrote:

but when I look at the pins attached and at the datasheet of my microcontroller, pins for USART3 on the MCU are not PC11 and PC10.  !


Yes, they are:

AndrewNeil_0-1744102282872.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
EliazLBAuthor
Associate III
Apr 8, 2025 8:59 AM UTC

Yes thank you apparently I can't really read...

Mike_ST
Mike_STBest answer
ST Technical Moderator
Apr 8, 2025 8:53 AM UTC

Hello,

>> pins for USART3 on the MCU are not PC11 and PC10

 

Mike_ST_0-1744102086837.png

 

>> So my question is pretty simple, which document is right and which should I follow ?

Both are right,

>> Am I going to need to change anything

If you want to use the bootloader on USART3, probably you'll need to switch to PC10/PC11.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
EliazLBAuthor
Associate III
Apr 8, 2025 8:56 AM UTC

So the simple answer is I need to use pins indicated in AN2606 ?

 

Andrew Neil
Super User
Apr 8, 2025 9:00 AM UTC

Correct - that's why it specifically states them.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
EliazLBAuthor
Associate III
Apr 8, 2025 9:01 AM UTC

Alright perfect then, thank you very much !