Skip to main content
batist_2008
Associate II
May 3, 2012
Question

Bootloader and interrupts in user application

  • May 3, 2012
  • 4 replies
  • 815 views
Posted on May 03, 2012 at 16:08

Hello everyone!

Help me, please, to understand where is the problem. I have my own bootloader, located at 0x08000000. And user application I locate at 0x08019000. The algorithm of my bootloader is: 1.After reset I have timeout at about 5 sec.If the connection between MCU and PC throught flash loader demonstrator is set, I load program and reboot MCU by NVIC_SystemReset(). 2. If there is no connection between MCU and PC and5 sec left I load user application. I use for connection between MCU and PC USART2. And in user application I want to use it too, but in another way. It is all right when I load symple programm which does notuse interrupts, it works correctly. But when I load programm that use USART2 and interrupts from USART2 the programm doesn't work. The code is:

void JumpToApplication (uint32_t ApplicationAddress) 
{ 
typedef void (*pFunction)(void); 
pFunction Jump_To_Application; 
uint32_t JumpAddress; 
NVIC_SetVectorTable(NVIC_VectTab_FLASH, USER_PROG_OFFSET); 
if (((*(__IO uint32_t*)ApplicationAddress) & 0x2FFE0000 ) == 0x20000000) //Провер�?ем, е�?ть ли что-нибудь по адре�?у (там должно лежать значение SP дл�? приложени�?, его кладет линкер) 
{ 
JumpAddress = *(__IO uint32_t*) (ApplicationAddress + 4); //�?дре�? перехода из вектора Reset 
Jump_To_Application = (pFunction) JumpAddress; //Указатель на функцию перехода 
__set_MSP(*(__IO uint32_t*) ApplicationAddress); //У�?танавливаем SP приложени�? 
Jump_To_Application(); //Запу�?каем приложение 
} 
} 
/*====================================================================================================*/ 
int main (void) 
{ 
InitBootCLK(); 
InitTimer(TIM2, 100000);//4�?ек 
NVICTmrInit(TIM2,TIM2_IRQn,1); 
InitUSARTPeriph(USART_SPEED,USART_Pins,BOOT_USART,USART_Interrupt); 
TmrOn(TIM2); 
TIM_ITConfig(TIM2,TIM_IT_Update,ENABLE); 
while (!BootLoaderStack.TIMEOUT_FLAG){} //ждем 4 �?екунды по�?ле запу�?ка 
switch (BootLoaderStack.TIMEOUT_FLAG) 
{ 
case TIMER_SRC: { 
AppAddr=((ReadFromFlash(PRG_ADDR_CELL)<<
16
)|ReadFromFlash(PRG_ADDR_CELL+2));//+USER_PROG_OFFSET; 
if (((AppAddr>=FLASH_START_ADDR)&&(AppAddr<=FLASH_END_ADDR))||((AppAddr>=SRAM_START_ADDR)&&(AppAddr<=SRAM_END_ADDR))) 
{ 
RCC->APB1RSTR=0; 
RCC->APB2RSTR=0; 
RCC->APB1ENR=0; 
RCC->APB2ENR=0; 
TmrOff(TIM2); 
TIM_ITConfig(TIM2,TIM_IT_Update,DISABLE); 
USART_Cmd(USART2,DISABLE); 
USART_DeInit(USART2); 
USART_ITConfig(USART2,USART_IT_TC,DISABLE); 
USART_ITConfig(USART2,USART_IT_RXNE,DISABLE); */ 
__disable_irq (); 
JumpToApplication(AppAddr); 
} 
else 
{ 
while (1) 
{ 
BootLoaderProcessing(); 
if (BootLoaderStack.APPLICATION_READY_FLAG) 
NVIC_SystemReset(); 
} 
} 
break; 
case BOOT_SRC: 
{ 
while (1) 
{ 
BootLoaderProcessing(); 
if (BootLoaderStack.APPLICATION_READY_FLAG) 
NVIC_SystemReset(); 
} 
} break; 
default: break; 
} } 

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    May 3, 2012
    Posted on May 03, 2012 at 19:23

    Interrupt should still be workable, as long as the vector table is correct, and the core knows where it is. I needs to be on a 512-byte boundary.

    To be honest you could delay for 4 seconds, and poll the serial port without using timer or usart interrupts.

    Break out the debugger and dig in.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    amin23
    Visitor II
    May 4, 2012
    Posted on May 04, 2012 at 19:28

    Hi,

    You should update the Vector Table base offset. For example, if your application start at 0x08004000, the vector table base offset should be 0x4000.

    to update VT go to system_stm32fxxx.c file and set VECT_TAB_OFFSET to 0x4000 or call NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x4000) function

    Tesla DeLorean
    Guru
    May 4, 2012
    Posted on May 04, 2012 at 21:58

    You should update the Vector Table base offset. For example, if your application start at 0x08004000, the vector table base offset should be 0x4000.

    to update VT go to system_stm32fxxx.c file and set VECT_TAB_OFFSET to 0x4000 or call NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x4000) function

    He does have

    NVIC_SetVectorTable(NVIC_VectTab_FLASH, USER_PROG_OFFSET); 

    I might just use NVIC_SetVectorTable(0x08019000, 0);
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    evert2
    Associate III
    December 6, 2012
    Posted on December 06, 2012 at 11:09

    Hi,

    Is the solution of this problem found yet?

    It seems like that I have the same issue with an STM32F051 microcontroller,

    Regards,

    Evert Huijben