Skip to main content
jedlb
Associate II
August 11, 2009
Question

BOOT0 pin

  • August 11, 2009
  • 3 replies
  • 831 views
Posted on August 11, 2009 at 17:15

BOOT0 pin

    This topic has been closed for replies.

    3 replies

    jedlb
    jedlbAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:20

    Hi All

    Is it possible to use BOOT0 (pin 60 of 64pin package)like general IO pin input?

    Thank you :-[

    swhite
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:20

    No.

    guyvo67
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:20

    Obviously not, the explanation lies in the pin name itself ''BOOT0''. It's dedicated to serve a predefined hardware behaviour on chip and is well documented in the specifications.

    Perhaps looking for 100-pins target if you're running low on free GPIOs ;)

    cheers

    Guy