Skip to main content
Associate III
Sep 18, 2025 12:00 PM UTC
Solved

Boot problem with STM32N6

I am having trouble connecting to the STM32N6 with SWD.

I have implemented a design using the STM32N645X0H3Q (though I have placed the STM32N647X0H3Q) using external VDDCORE. R110 is not mounted (to set VLXSMPS to NC).

On startup I have VDDIO (3.3V) and VDDA1V8ON (1.8V) to the MCU, and the MCU activated PWR_ON (I have VDDA1V8ON to the PDR_ON pin, A1 on another page). This activates the reset of the power, including VDDCORE. All voltage measurements are as expected on the board.

When I try to connect to the board using SWD in STMProgrammer (v2.20.0), I see the 3.3V, but the STMProgrammer does not connect. I am using a Minnie V3 (v V3J16M8) on Windows. I have tried lower frequencies and all modes and reset modes without success.

 

I should mention that on my prototype board, I have not mounted external crystals, flash or ram. Though I believe that is not necessary for STMProgrammer to see the MCU.

 

Any help is greatly appreciated!

edenrafBest answer
Associate III
Jun 12, 2026 6:28 AM UTC

Turns out I had my VDDA18AON mislabelled slightly so it never connected in the schematic. Crazy I missed that the 100s of times I reviewed the schematic

2 replies

edenrafAuthor
Associate III
Sep 22, 2025 7:06 AM UTC

I should also note that BOOT0 is at GND, and BOOT1 is at VDDIO. Though I have tried all of the possible configurations with the BOOT pins.

Again, any help is very welcome at this point!

edenrafAuthorBest answer
Associate III
Jun 12, 2026 6:28 AM UTC

Turns out I had my VDDA18AON mislabelled slightly so it never connected in the schematic. Crazy I missed that the 100s of times I reviewed the schematic