Skip to main content
VTOL_Aviations
Associate III
March 22, 2019
Question

Board: STM32F407G-DISC1, OS: ubuntu 16.04, IDE: Attolic TrueStudio, CubeMX(for code generation), Baud rate: 9600, Time Base Source : SysTick

  • March 22, 2019
  • 0 replies
  • 411 views

Hi,

I'm trying to receive data through USART2 through Arduino's serial terminal. I'm not able to receive anything. When I suspend the process, it is always stopping at UART_WaitOnFlagUntilTimeout(); . I'm using "HAL_UART_Receive(&huart2, rx_data, 10, HAL_MAX_DELAY)" function to receive data through serial terminal. I've kept rx_data as a watch expression. But I'm not able to observe anything. 

I'm also getting multiple errors in the "Expression" tab. The errors are:

Multiple errors reported.

1) Failed to execute MI command:

-var-create - * rx_data

Error message from debugger back end:

-var-create: unable to create variable object

NOTE: I haven't connected the usart to usb dongle. And i haven't connected flying wires from USART's Tx and Rx to ST-LINK's Tx and Rx.

My Code:

int main(void)

{

  

 HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();

 MX_USART2_UART_Init();

 uint8_t tx_data[10] = {1,2,3,4,5,6,7,8,9,10};

 uint8_t rx_data[10];

 //HAL_UART_Transmit(&huart2, tx_data, 10, HAL_MAX_DELAY);

 while (1)

 {

HAL_UART_Receive(&huart2, rx_data, 10, HAL_MAX_DELAY);

 }

}

Please guide.

This topic has been closed for replies.