Skip to main content
KKurt.1
Associate II
November 12, 2020
Question

BlueNRG-M2SP Device gets stuck at hci_tl_lowlevel_isr function

  • November 12, 2020
  • 4 replies
  • 1746 views

So I am trying to use BlueNRG M2SP device on a custom board. To use this device i tried to use BLE2 cube expansion with SampleApp application. I am sure i am configuring SPI and GPIO pins correctly. Project builds and loads fine but after booting, code gets in to a loop at here.

void hci_tl_lowlevel_isr(void)
{
 /* Call hci_notify_asynch_evt() */
 while(IsDataAvailable())
 {
 hci_notify_asynch_evt(NULL);
 }
 
 /* USER CODE BEGIN hci_tl_lowlevel_isr */
 
 /* USER CODE END hci_tl_lowlevel_isr */
}

I tried to comment out this section of the code just to see what happens, and BLE doesnt get initiated correctly if i do that.

I will be glad if someone can be helpfull.

Koksal

This topic has been closed for replies.

4 replies

BLin.3
Associate
November 19, 2020

@Köksal Kurt​ Any updates on this?

KKurt.1
KKurt.1Author
Associate II
November 19, 2020

@BLin.3​   Yeah i managed the solve the problem. Firstly you have to upload correct firmware for BNRG device. It can be done using BlueNRG Flasher utility.

Also in my PCB i was using DIO1 pin for CS line. But that was wrong. CS pin should always be DIO11 pin.

Those fixes solved my issue.

BLin.3
Associate
November 19, 2020

@Köksal Kurt​ thanks for the reply! When you said correct firmware, did you mean the DTM_SPI firmware?

Wingunder
Associate III
December 22, 2020

Hi KKurt.1,

I had the same problem, and it turned out to be a interrupt pin miss-configuration.

Refer to the following schematic:

https://www.st.com/content/ccc/resource/technical/layouts_and_diagrams/schematic_pack/group1/71/cf/2c/3a/24/07/42/7b/X-NUCLEO-BNRG2A1_SCHEMATIC/files/x-nucleo-bnrg2a1_schematic.pdf/jcr:content/translations/en.x-nucleo-bnrg2a1_schematic.pdf

The PA0_SPI_IRQ must be wired correctly to your host-processor.

If you are using the X-NUCLEO-BNRG2A1, then it is important to note that the board was populated with:

  1. PA0_SPI_IRQ_PB14_BNRG1BOOT connected to PA0, with R85 (0 Ohm)
  2. PA0_SPI_IRQ_PB14_BNRG1BOOT connected to PB14, with R82 (0 Ohm)

Unfortunately PB14 is also the JTAG CLK (SWCLK)! This means that you'll have no chance to try and debug your host-processor's application unless you remove PB14. So, take care. I have no idea why the designers of this board populated R82. A possible explanation could be that there was a manufacturing mix-up and R82 got populated, instead of R117.

So, in short: Remove the 0 Ohm resistor from R82 and solder it to R117.

Now, you should be able to debug with SWCLK and if your PA0's interrupt is enabled in the host-processor's software, it should just work.

Regards