Skip to main content
michelemancini2
Associate III
December 13, 2021
Question

BlueNRG_LP multiple channel ADC

  • December 13, 2021
  • 2 replies
  • 762 views

I am working with BlueNRG LP.

I am acquiring 3 channels:

ADC_VINP0 (PB3)

ADC_VINM0 (PB2)

BATTERY.

I used and modified example of the "BlueNRG-LP Navigator" ADC_DMA.

I read ADC_VINP0 and the batteries but ADC_VINM0 not work!! ( I used STEVAL-IDB011V1 and i remove the "R50" (pin DOUT of MP34DT05-A digital microphone)

static void MX_ADC_Init(void)
{
 /* Enable the ADC peripheral */
 HAL_ADC_StructInit(&adc_handle);
 adc_handle.Init.DataRatio = USER_RATIO;
 adc_handle.Init.DataWidth = USER_DATAWIDTH;
 adc_handle.Init.SampleRate = USER_SAMPLERATE;
 adc_handle.Init.SamplingMode = ADC_SAMPLING_AT_START; 
 adc_handle.Init.SequenceLength = ADC_SEQ_LEN_03;
 adc_handle.DMA_Handle = &hdma_adc;
 
 if (HAL_ADC_Init(&adc_handle) != HAL_OK) {
 Error_Handler();
 }
 
 /* Set the 1 input channel */
 xChannel.ChannelType = ADC_CH_VINP0_TO_SINGLE_POSITIVE_INPUT;
 xChannel.SequenceNumber = ADC_SEQ_POS_01;
 xChannel.VoltRange = ADC_VIN_RANGE_3V6;
 if (HAL_ADC_ConfigChannel(&adc_handle, &xChannel)!= HAL_OK) {
 Error_Handler();
 }
 
 
 /* Set the 2 input channel */
 xChannel.ChannelType = ADC_CH_VINM0_TO_SINGLE_NEGATIVE_INPUT; 
 xChannel.SequenceNumber = ADC_SEQ_POS_02;
 xChannel.VoltRange = ADC_VIN_RANGE_3V6;
 if (HAL_ADC_ConfigChannel(&adc_handle, &xChannel)!= HAL_OK) {
 Error_Handler();
 }
 
 /* Set the 3 input channel */
 xChannel.ChannelType = ADC_CH_BATTERY_LEVEL_DETECTOR;
 xChannel.SequenceNumber = ADC_SEQ_POS_03;
 xChannel.VoltRange = ADC_VIN_RANGE_3V6;
 if (HAL_ADC_ConfigChannel(&adc_handle, &xChannel)!= HAL_OK) {
 Error_Handler();
 }
 
 
 
 LL_ADC_SetCalibPoint1Gain(ADC, LL_ADC_DEFAULT_RANGE_VALUE_3V6);
 LL_ADC_SetCalibPointForSinglePos3V6(ADC, LL_ADC_CALIB_POINT_1);
}
 
/** 
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void) 
{
 /* DMA controller clock enable */
 __HAL_RCC_DMA_CLK_ENABLE();
 
 /* Configure NVIC for DMA */
 HAL_NVIC_SetPriority(DMA_IRQn, 0);
 HAL_NVIC_EnableIRQ(DMA_IRQn);
 
}

This topic has been closed for replies.

2 replies

TDK
December 13, 2021

> ADC_VINM0 not work

What about it doesn't work? What results are you getting and what do you expect instead?

"If you feel a post has answered your question, please click ""Accept as Solution""."
michelemancini2
Associate III
December 13, 2021

i found the problem, i got confused with the HAL and LL drivers