Skip to main content
per3
Associate III
March 4, 2008
Question

blocking downloading

  • March 4, 2008
  • 2 replies
  • 710 views
Posted on March 04, 2008 at 10:39

blocking downloading

    This topic has been closed for replies.

    2 replies

    jilisegiar
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:25

    Rlink configuration-> advanced options->click here to open option dialog box

    and set the ''read out protection'' option then click on ''write target Option Bytes now'' button.

    per3
    per3Author
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:25

    I have Raisonance RIDE 7. On the options there I see I can download the target code into a hex file.

    This makes me wonder, is there some setting to do to prevevent this, just like they have in Atmelk AVR devices - you set a bit to block reading of the code.

    Simply put, how do you prevent stealing of production code once you ship units?