Skip to main content
Gpeti
Senior
Feb 9, 2024 9:09 AM UTC
Question

Bit SCUEN of PWR peripheral of STM32H7

We don't understand the bit SCUEN of STM32H7.

 

The description is not very clear:

 

Gpeti_0-1707468529159.png

 

Gpeti_1-1707468601674.png

 

Could you explain what SCUEN means and if the software is supposed to write or read this bit and why ?

This topic has been closed for replies.

5 replies

Lead II
Feb 10, 2024 4:46 AM UTC

Where have you seen this? I tried to find in my STM32H7 manuals but I do not see anything for SCUEN.

Where is coming from? (provide doc name, link and page as info, thank you).

Gpeti
GpetiAuthor
Senior
Feb 12, 2024 7:02 AM UTC

It's in the technical reference manual, nothing exotic...

Chapter 6 "PWR"

LCE
Principal III
Feb 12, 2024 8:05 AM UTC

No SCUEN bit in RM0468 for STM32H723/733, STM32H725/735 and STM32H730

LCE
Principal III
Feb 12, 2024 11:44 AM UTC

Okay, RM0433.

You should always say which STM32 / H7 exactly you are using, even in the "basic" registers there seem to be some differences between the H7 types.

I would check how the HAL libraries are using this bit, if they are using it all.