Skip to main content
PGild.1
Associate III
May 24, 2023
Solved

Bit-banged I2S on STM32F103

Hello everybody,

I am trying to bit-bang an I2S interface on an STM32F103 at 72MHz using TIM2.

Am I way too optimistic to get a 3MHz "clock" out on a pin? The fastest I can seem to get it is at 90kHz.

I have set the "prescaler" of TIM2 to "0" and "1".

And, I have set the auto reload register at 11 with an interrupt writing "0" and "1" to a GPIO pin.

And Channel 1 set as "Output comapre no output" as well as "PWM1 output" on PA15.

The CPU and timer frequencies are 72MHz.

Any suggestions? (other than get an STM32 with I2S ;) )

Kind regards,

pieterg!

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 24, 2023

Well, there are some users who torture themselves with the emulation of I2S. However, it should be possible to emulate I2S with the STM32F103 as well, as a search with your favourite search engine for e.g. "+I2S +emulation +STM32" will reveal.

Among other things, you should then also find the AN5086, which deals with the topic and implements it with SPI and a timer on a Cortex-M0 (STM32L0).

There is also a bare-metal idea with an STM32F1 here.

Maybe that will help you?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

4 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
May 24, 2023

Well, there are some users who torture themselves with the emulation of I2S. However, it should be possible to emulate I2S with the STM32F103 as well, as a search with your favourite search engine for e.g. "+I2S +emulation +STM32" will reveal.

Among other things, you should then also find the AN5086, which deals with the topic and implements it with SPI and a timer on a Cortex-M0 (STM32L0).

There is also a bare-metal idea with an STM32F1 here.

Maybe that will help you?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PGild.1
PGild.1Author
Associate III
May 26, 2023

Hello Peter,

Thank you so much for the quick response!

I have followed the application and the logic analyser results looks very promising.

I see a 2.286MHz clock now (as expected for the CubeMX settings) and I have the "WS" signal from a timer as per the application note.

Kind Regards,

pieterg!

Peter BENSCH
ST Technical Moderator
May 26, 2023

Great!

When the problem will be solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.