Skip to main content
sima
Associate III
February 14, 2009
Question

Bit banding SRAM when booting from SRAM?

  • February 14, 2009
  • 2 replies
  • 564 views
Posted on February 14, 2009 at 05:07

Bit banding SRAM when booting from SRAM?

    This topic has been closed for replies.

    2 replies

    sima
    simaAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:02

    Does the bit band alias base address for the SRAM (0x22000000) change to 0x02000000 if I select to boot from system memory block (SRAM)?

    I have read that the SRAM will appear at 0x00000000 if embedded SRAM is selected as boot space.

    joseph239955
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:02

    No, it doesn't. The bit-band is fixed at 0x22000000 and 0x42000000. If the memory is remapped to 0x0 by the memory system, the processor will not carry out bit-band operation to it.