Skip to main content
asterix
Associate III
January 9, 2008
Question

Big endian and Little endian ?

Posted on January 09, 2008 at 18:05

Big endian and Little endian ?

    This topic has been closed for replies.

    5 replies

    edware
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Hi Magigimix,

    Here's a quote from the Arm M3 Cortex Technical Reference Manual:

    Quote:

    The processor can access data words in memory in little-endian format or big-endian format. It always accesses code in little-endian format.

    Note

    Little-endian is the default memory format for ARM processors.

    ...

    The processor contains a configuration pin, BIGEND, that enables you to select either the little-endian or BE-8 big-endian format. This configuration pin is sampled on reset.

    You cannot change endianness when out of reset.

    I hope you still have some hair left!

    Regards

    edware

    HDaji.1
    Senior
    November 20, 2023

    "some hair left" is the reason I thumbed it up. :D

    asterix
    asterixAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Hi Folks,

    I am tearing my hair out on this one and hoping someone can help :

    is STM32 ( Cortex-M3) Little or Big endian and how we can change it at both processor level and in keil or IAR compiler options ? :-?

    Thanks , Magigimix

    asterix
    asterixAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    Dear edware,

    Thanks so much , I still have some :) last night.

    back to your answer and to conclude : I can change at reset the data endianess only, but how ? I can not see any pin called BIGEND. Thx again.

    kind regards, Magigimix

    sjo
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:20

    No you cannot change the endianess, it is little endian only.

    The BIGEND is an internal setting to the cortex die.

    Cheers

    Spen