Skip to main content
Kent Swan
Associate III
August 7, 2018
Question

BIG BUG - CubeMX, STM32L476 and USB OTG Device Only and HAL_GPIO_EXTI_Callback

  • August 7, 2018
  • 3 replies
  • 612 views

STM32L476 with STM32Cube_FW_L4_V1.12.0. Configuring for Device only OTG, CubeMX ALWAYS generates HAL_GPIO_EXTI_Callback in usbd_conf.c for VBUSDetect. This HAL_GPIO_EXTI_Callback generated code does not have any USER CODE BEGIN... USER CODE END construct. This means that this generated code HOGS the HAL_GPIO_EXTI_Callback and does not permit any other EXTI actions to be stably implemented within the callback.

RULE 1: It is not permissible for a single generated peripheral pin function (such as HAL_GPIO_EXTI_Callback) in a way that additional normal usage of that function is blocked in a way that you cannot add the other usages of the function in a stable manner.

    This topic has been closed for replies.

    3 replies

    Kent Swan
    Kent SwanAuthor
    Associate III
    August 7, 2018

    More bad news. HAL_GPIO_EXTI_Callback for VBUSDetect is generated without regard to the enable/disable selections in CubeMX. Means that this CubeMX implentation is badly broken.

    Kent Swan
    Kent SwanAuthor
    Associate III
    August 8, 2018

    Observation: HAL_GPIO_EXTI_Callback should probably be generated in main() and include the normal USER CODE blocks so that additional defined EXTI pins can be reliably incorporated without undue strain.

    Kent Swan
    Kent SwanAuthor
    Associate III
    August 9, 2018

    WORK AROUND!!!!!

    Found a workaround to CubeMX not generating the HAL_GPIO_EXTI_Callback in usbd_conf.c with USER CODE blocks to allow extension. The following is a stable hack under CubeMX regeneration.

    1. At the top of usbd_conf.c in USER CODE 0 block add the following
    • #undef HAL_GPIO_EXTI_Callback
      • #define HAL_GPIO_EXTI_Callback HAL_GPIO_EXTI_Callback_VUSBDetect

    2. Where ever you implement HAL_GPIO_EXTI_Callback add the following inside that code

    HAL_GPIO_EXTI_Callback_VBUSDetect(GPIO_Pin);

    What this does is renames the improperly defined HAL_GPIO_EXTI_Callback to HAL_GPIO_EXTI_Callback_VBUSDetect in a way that compiles and links properly even when code is regnerated and thus allows you to add the additional EXTI captures in a stable manner