Best way to interface to external ADCs like TI's ADS1232?
There is a plethora of 24-bit ADCs similar to TI's ADS1232, which output data using a "DREADY/DOUT" pin and expect the micro to supply a variable number of clock pulses depending on the operation (read / calibrate / write, etc).
These are typically low bandwidth, high ENOB devices for medical and other precision applications.
What is the best way to interface to these from STM32 silicon? Is it worth trying to cajole the SPI bus to conform to this behavior, or should I just forget about it and bit-bang the whole thing? Searching the forums didn't reveal much.
Thanks.