Senior II
March 12, 2023
Solved
Best ADC accuracy that can be obtained with a Nucleo board or similar.
- 19 replies
- 11699 views
I am using STM32F407 and STM32F767ZI on Nucleo and other boards. My configuration is a simple potentiometer as voltage divider (200K or 1K) to generate the analog input voltage.
Even with stable voltage on the ADC input (verified with my fluke 117 & Picoscope 5000, 2,000V, delta < 5mV), the values read on the ADC vary over ranges of about 100mV (0,117mV).
My question:
1) What is a typical accuracy one can expect on such a simple configuration.
2) What is the major contributor to this inaccuracy, and what can be done about it.
Note:
Detailed analysis added as an attachement.