Skip to main content
Associate III
Jan 6, 2026 7:26 AM UTC
Question

Beginner example for DCMIPP on STM32N6570DK

Hello, I wanna use the development board STM32N6570-DK for taking a picture with MB1854B. i am quite new for DCMI and DCMIPP. i just want to read the image through the pipe1 of dcmipp but i dont know how to config the MCU in .ioc file. Can anyone explain or give me an example for that? 

3 replies

ST Technical Moderator
Jan 6, 2026 8:00 AM UTC

Hello @pawatJoy ,

You can follow the steps and configuration for DCMIPP examples based on STM32CubeMX:

You can also refer to the github example shows how to use the DCMIPP IP based on the STM32Cube HAL that can be used to build any firmware application:

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
pawatJoyAuthor
Associate III
Jan 7, 2026 11:17 AM UTC

Hello again,

 

i have read the AN6211 and walked through the code in DCMIPP_SnapshotDecimationMode. it appeared that it required  #include "isp_api.h". in the main.h.

 

Where should i find that files and how do i install that in stmCubeIDE? 

Associate
Apr 2, 2026 5:37 PM UTC

Hello

I was reading different questions about DCMIPP configuration to see if I could find an answer to my problem. I came across this question, it may be too late. Anyway, you should copy the ISP library into your porject: you can find it in C:\Users\username\STM32Cube\Repository\STM32Cube_FW_N6_V1.3.0\Middlewares\ST. The version of STM32CUBE_FW_N6 depends on the version you use in stmcubeMX. Also you have to copy the drivers in C:\Users\username\STM32Cube\Repository\STM32Cube_FW_N6_V1.3.0\Drivers\BSP. For camera module IMX335 you need: imx335 
DM if you want the ioc configuration, I am not sure if it is completely correct, but it may help

Spoiler