Skip to main content
JPiet.3
Associate III
October 12, 2023
Solved

BDSL File for STM32H745XIH6

Hello,

is somebody is knowing, if a BDSL-File for  STM32H745XIH6  is existing? The affected processor doesn't exist in the "en.stm32h7_bsdl.zip" (https://www.st.com/resource/en/bsdl_model/stm32h7_bsdl.zip) from STM. Five packages are supported, but not the TBGA256.

I would be happy, if someone can share a link or a file with me.

Thanks,

Jan

This topic has been closed for replies.
ELABI.1
ELABI.1Best answer
ST Technical Moderator
October 12, 2023

Hello @JPiet.3,

The STM32H745XIH6 is an MCU from TFBGA 240+25 package.

Please refer to the datasheet, specifically "8 Ordering information section" for more information. I have attached the Datasheet link.

The BSDL of STM32H745XIH6 is already exist in zip file with "STM32H745_755_TFBGA240" file name.

Thank you.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Eya.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

ELABI.1
ELABI.1Best answer
ST Technical Moderator
October 12, 2023

Hello @JPiet.3,

The STM32H745XIH6 is an MCU from TFBGA 240+25 package.

Please refer to the datasheet, specifically "8 Ordering information section" for more information. I have attached the Datasheet link.

The BSDL of STM32H745XIH6 is already exist in zip file with "STM32H745_755_TFBGA240" file name.

Thank you.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Eya.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.