Question
Basic timer questions STM32L476?
Hello all...
Can someone give me direct answers below...(And please don't refer me to documentation as I have scoured thru it and not solved my questions)
I would like some clarity as I have found no documentation to clarify the following:
- When using compare output and pwm for triggering other timers does RCR have any affect? or does RCR only affect UG?
- When a timer is configured to use ITRx and in slave mode and NOT External Clock Source does the timer automatically just use the internal clock source?
- I have yet to find the value of TG in EGR as no one has taken the time to show a Figure wrt to this topic....Can anyone tell me it's value?
- I cannot make heads or tails from what ST is trying to say in the UM Figure 376....What are they trying to show here? CNT_INIT??? this is the only place in the whole RM this is mentioned. The paragraph before the figure is almost as incomprehensible....UG signal here doesn't seem to align with anything going on within the figure???
- Finally UG and TG.....what are their value? Doesn't everyone use interrupts? in particular the Update Event in Trigger Selection, is this tied to UG????
ST documentation is very poor with respect to labeling and consistency. They could do a whole bunch better if they stuck with using the register names and bit field names throughout their documentation especially on figures......
Sincerely