Skip to main content
danielblesener9
Associate III
April 15, 2013
Question

Basic - starting project for stm32F1 from scratch w/ Ride7

  • April 15, 2013
  • 2 replies
  • 595 views
Posted on April 16, 2013 at 01:27

I have created many projects using Ride7 for the STM32F1, but I always have started with example projects from ST. I need to start from scratch.

I simply created a project, and only added stm32f10x_rcc.h and .c partner.  Since I am using the default script and start file, I figured the start should be as easy as settings a few clocks. I am getting the error message ''W:\Public\Dan\Actuator Testing Design\Firmware\700-1221 Relay Testing Board Rev1.00\Relay Testing Board Rev 1.00.elf: file not recognized: File truncated''

Also, above that the end of the line says nostartfiles.

I am sure the start files and script files exist though. Any idea what I am doing wrong?

Thanks
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    April 16, 2013
    Posted on April 16, 2013 at 02:10

    Not a Ride user, but you should perhaps check the .MAP file and see how that contrasts to working projects. Make sure it's pulling in startup_stm32f1xx.s (or equivalent), and it has a vector table.

    Generally when making new projects you have to make sure the compiler has a list of include directory paths (-I), and preprocessor defines (-D). These kinds of things can be specified at a project or file level, but usually hidden within the metadata of the project file itself. If the tools can generate a makefile, compare/contrast those between working/non-working examples.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    danielblesener9
    Associate III
    April 16, 2013
    Posted on April 16, 2013 at 20:40

    Perfect! Problem solved, thanks much!