Skip to main content
xtian
Associate III
January 17, 2013
Question

BASIC GPIO

  • January 17, 2013
  • 7 replies
  • 2053 views
Posted on January 17, 2013 at 09:34

Hi Guys,

I am 1week old to stm32 programming I came from PIC

1ST QUESTION

// FROM Pic Basic Code normally I do this

TrisC = %11111111

int data = PortC

the return is the decimal equivalent of the binary or port C example 1000001 data will contain 65 then that is very easy to manipulate if you want to send via USART / LCD

//00: General purpose output push-pull

//01: Output mode, max speed 10 MHz.

 GPIOC->CRL = 0x11111111;

 GPIOC->CRH = 0x11111111;

//10: Input with pull-up / pull-down

//00: Input mode (reset state)

// set as pulldown

  GPIOA->CRL = 0x88888888;

  GPIOA->CRH = 0x88888888;

  GPIOA->ODR = 0x0000;

while(1)

{

    GPIOC->BSRR |= GPIO_ReadInputData(GPIOA);  //read pins and set PORTC from data of PORTA

    GPIOC->BRR |= GPIO_ReadInputData(GPIOA);  //reset portC based from portA

}

this is working but i want to convert the data to 8 bit to represent an ascii

i want a concept that is similar to this

int data = GPIO_ReadInputData(GPIOA);

instead of doing this:

if (GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_6) == 1)

    {

     data +=64

   }

(GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_5) == 1)

    {

     data +=32

   }

(GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_4) == 1)

    {

     data +=16

   }

2ND QUESTION

usually in PIC to declare a input and output

I DO THIS

TRISA = %11110000 //1111input 0000output so port0-port3(output) port4-port7(input)

so in STM32VL for example i want port A0 - portA7 as output and the rest A8-AX as input how do i do that?

    This topic has been closed for replies.

    7 replies

    Tesla DeLorean
    Guru
    January 17, 2013
    Posted on January 17, 2013 at 23:21

    int data = GPIO_ReadInputData(GPIOA) & 0xFF; // Will mask low order bits

    int data = GPIOA->IDR & 0xFF; // A more direct form

    The LCD code is done in a bitwise fashion to allow an agnostic implementation, where the pins are scattered, or in reverse order, or whatever.

      /* GPIOA Periph clock enable */

      RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

      /* Configure PA0 .. PA7 in output pushpull mode */

      GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;

      GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

      GPIO_Init(GPIOA, &GPIO_InitStructure);

      /* Configure PA8 .. PA15 in input, pulled up mode */

      GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;

      GPIO_Init(GPIOA, &GPIO_InitStructure);

      GPIOA->ODR = GPIOA->IDR >> 8; // Mirror high ordered inputs to low ordered outputs

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    xtian
    xtianAuthor
    Associate III
    January 18, 2013
    Posted on January 18, 2013 at 01:48

    Hi Clide,

    Thank you very much! your the best:) This gave me a good start to understand configuring pins in C. may I ask if you have a spare time this weekend and if you could give me a crash course just teach me how to start and  that's it the rest I'll manage...:)

    I am trying to study on my own but it may stil take 2-4 weeks and my project is due this january 31. I hope you could be my mentor for at least 3-4 hours or for the basics of C in STM programming

    xtian
    xtianAuthor
    Associate III
    January 18, 2013
    Posted on January 18, 2013 at 02:18

    typedef struct

    {

      uint16_t GPIO_Pin;         

      GPIOSpeed_TypeDef GPIO_Speed;

      GPIOMode_TypeDef GPIO_Mode;

    }GPIO_InitTypeDef;

    is this one

    GPIO_InitTypeDef GPIO_InitStructure; like creating an object of a class which allows me to use its variable or methods?

    GPIO_InitTypeDef - class

    GPIO_InitStructure - object / variable

    so I can make it something like GPIO_Initialization

    xtian
    xtianAuthor
    Associate III
    January 18, 2013
    Posted on January 18, 2013 at 02:28

    Please see if my understanding are correct

    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7;

    //will put implement the succeeding lines on the following pins 0, 1, 2,3,4,5,6,7

      GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

    //will put implement the a 50 mhz cycle on pins 0, 1, 2,3,4,5,6,7

     

      GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

    //will put implement a push pull on pins 0, 1, 2,3,4,5,6,7

      GPIO_Init(GPIOA, &GPIO_InitStructure);

    //will implement all the setting above on portA

    //so if i have some thing likeGPIO_Init(GPIOC, &GPIO_InitStructure); settings above will //also be implemented to portC pins 0-7

    Tesla DeLorean
    Guru
    January 18, 2013
    Posted on January 18, 2013 at 02:55

    type

    structure

    GPIO_Init() is a function that takes a pointer to the structure (array in memory if you will) that contains the setting we want to apply.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    xtian
    xtianAuthor
    Associate III
    January 18, 2013
    Posted on January 18, 2013 at 02:57

    thanks clide!

    xtian
    xtianAuthor
    Associate III
    January 18, 2013
    Posted on January 18, 2013 at 03:04

    Thanks clive! how I wish you are the Philippines so I could treat you :) how about it clive do you have some spare time? could I have you as a mentor for few hours?