Skip to main content
BFalcon
Associate II
February 28, 2020
Question

B-G431B-ESC1 20vdc Max?

  • February 28, 2020
  • 9 replies
  • 2092 views

Oddly the on board NFETS are rated 60v, why only 20v input? Can we safely go to +48vdc, if not why? Our motor driven FW the voltage does not go above Vbus.

Is FOC space vector 7 phase or 5 phase switched?

Thanks

This topic has been closed for replies.

9 replies

BFalcon
BFalconAuthor
Associate II
March 3, 2020

Anybody at ST knows why 20v is the rated bus voltage for the kit?

Ozone
Principal
March 3, 2020

At least the L7986 step-down regulator (U9) is only specified up to 38V.

BFalcon
BFalconAuthor
Associate II
March 4, 2020

Hard to imagine only 38v when the market has gone to 48v on almost all motor drives.

waclawek.jan
Super User
March 3, 2020

There's a 26V TVS right at the input...

I'd say the capacitors' rating may be limiting, too.

Maybe you want to contact ST directly, through web support form or through FAE.

JW

waclawek.jan
Super User
March 3, 2020

From the BOM:

C27 C28 C29 C30 C31 C32 C33 C34 C35 C36 C37 C38 C39 C40

15uFCAP CER 15UF 35V X5R 0805

There may be other critical capacitor, too.

The BAT30 Schottky is 30V rated; I'm not sure whether that's limiting or not.

JW

BFalcon
BFalconAuthor
Associate II
March 4, 2020

Perhaps it's more of a hobby EVM targeted for 20v drone motors.

waclawek.jan
Super User
March 4, 2020

Yes, but as you've hinted, it's a pity.

48V is maybe a bit much, but 24V (nominally; in fact it's more up to 30V) is quite common in industrial and semi-industrial settings. With a bit of attention, the board's utility might've been extended.

JW

Saurabh SONA
Visitor II
March 9, 2020

Going by the listed specs and size, the board indeed seems to be designed specifically for RC Drone applications powered by up to 6S LiPo battery packs.

The form factor required for these applications may be hard to meet with higher voltage rated capacitors etc.

For higher voltage ratings there is already X-NUCLEO-IHM08M1 (48V max) which can be used with NUCLEO-G431RB or other NUCLEO boards.

EWu.1
Associate
June 22, 2020

BEMF may double the VCC so it can not use in DC 48V, If you want to work under 48V .That need to modify all Schematch

​