Skip to main content
Anand A
Associate II
Jun 6, 2017 4:56 AM UTC
Solved

Availabiltiy of user data bytes in option bytes area in STM32L4 series

Posted on June 06, 2017 at 06:56

In STM32F3 series, user data bytes are available at location 0x1FFFF804. I have used this for storing a  status marker value. During power on reset i am checking this location based on the value I am executing some functions(I will changing this value in run time).  Is this feature available in STM32L4 series? I didn't find this in user manual.

    This topic has been closed for replies.
    Viktor POHORELY
    Viktor POHORELYBest answer
    ST Employee
    Jun 7, 2017 4:00 PM UTC
    Posted on June 07, 2017 at 18:00

    There is no dedicated user data byte in the option registers. You could use either backup registers or SRAM2, but both requires external backup capacitor or battery.

    Please note that using flash to store the state of the state machine has limits in the memory endurance.

    2 replies

    Viktor POHORELY
    Viktor POHORELYBest answer
    ST Employee
    Jun 7, 2017 4:00 PM UTC
    Posted on June 07, 2017 at 18:00

    There is no dedicated user data byte in the option registers. You could use either backup registers or SRAM2, but both requires external backup capacitor or battery.

    Please note that using flash to store the state of the state machine has limits in the memory endurance.

    AndyJT
    Associate III
    Feb 7, 2018 10:08 AM UTC
    Posted on February 07, 2018 at 11:08

    I was searching for an answer to this myself.

    I have a few bytes to store on a simple STM32L476 application.

    I don't want to have to fit any external components like batteries, super caps or EEproms etc.

    I appears that my only solution is to use bank 1 of Flash for program (512Kb) and bank 2 for my non-volatile setting bytes, of which I'll have more than 500 thousand to choose from !