Skip to main content
Associate
August 9, 2024
Question

Automatic SPI communication using STM32U5

Hi

I use STM32U575I-EV.

I want to periodically read data from an external SPI device without CPU.

The SPI device will emit a data ready signal(active low gpio), so I want to use that as a trigger to read the data.

Ideally, I would like to perform multiple SPI receptions while keeping the CPU in Stop mode.

To read data from a SPI device, just do something like HAL_SPI_Receive_DMA().

 

Are there any good example projects ?

Or how can I do this ?

I read this articles, but it didn't solve my problem.

Solved: STM32U5 SPI Continuous Communication - STMicroelectronics Community

Best regards.

This topic has been closed for replies.

2 replies

Amel NASRI
ST Technical Moderator
August 9, 2024

Hi @DK3 ,

I believe that the LPBAM is the good solution for your case.

To know more about the LPBAM, please refer to the wiki article Getting started with LPBAM.

As stated there, a typical example is provided in STM32Cube\Repository\STM32Cube_FW_U5\Projects\NUCLEO-U575ZI-Q\Applications\LPBAM\LPBAM_SPI_TransmitReceive. You can check the readme file to understand more the example.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
DK3Author
Associate
August 13, 2024

Hi, @Amel NASRI 

Thanks to your advices, I was able to do SPI read automatically.

I want to generate a DMA interrupt once every two times and use the receive buffer continuously.

(e.g. Receive1 uses RxBuff[0] ~ RxBuff[7], Receive2 uses RxBuff[8] ~ RxBuff[15])

So, I created two SPI_Receives as shown in the attached image and configured "Transfer Event Generation" as follows.

Receive1 : Transfer Event Generation = TC and HT generated on the last linked-list item

Receive2 : Transfer Event Generation = TC and HT generated on each block

DK3_0-1723540839321.png

This worked as intended. 

Is this setting correct ? Is there a better way ?

When I set Transfer Event Generation of Receive1 and Receive2 to TC and HT generated on the last linked-list item, DMA interrupt was not generated.

The latter setting seemed like the correct setting, but it didn't work.

Please tell me that reason.

Best regards.