Skip to main content
darkfirefighter
Associate II
Aug 26, 2010 12:16 PM UTC
Question

Assembler parameters for routine

Posted on August 26, 2010 at 14:16

Assembler parameters for routine

    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    May 17, 2011 12:04 PM UTC
    Posted on May 17, 2011 at 14:04

    Not sure your first example is correct. The value in R0 would be the integer ''i'', it is not a pointer. And loading from an address like ''5'' would cause a bus fault as it is unaligned.

    For your second

        LDR r1,[R0, #0] ; ar[0]

        LDR r2,[R0, #4] ; ar[1]

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    darkfirefighter
    Associate II
    May 17, 2011 12:04 PM UTC
    Posted on May 17, 2011 at 14:04

    To my first example:

    If I write LDR r1,r0

    i get a compiler error

    To the second:

    Great thanks it works fine :)

    Is there a an other way to incremet the pointer? Something like r0++?

    Or other said is this LDR r1,[r0,#0] the fastest way to access the array element 0?

    Thank your for your great help! :)

    picguy2
    Associate III
    May 17, 2011 12:04 PM UTC
    Posted on May 17, 2011 at 14:04

       ldr  r1,[r0]

       ldrh r1,[r0]

       ldrb r1,[r0]

       ldr  r1,[r0],#n

       ldrh r1,[r0],#n

       ldrb r1,[r0],#n

    The first 3 instructions are the basic memory loads.  The second 3 add n to the address register after the instruction.  The corresponding stores work the same way.  I don’t know if #-4 would work.  See if the assembler likes it.

    I believe the last 3 are 32-bit instructions but don’t know for sure.  My guess is that instructions with the #n take no longer to execute than those without #n.
    damh
    Associate III
    May 17, 2011 12:04 PM UTC
    Posted on May 17, 2011 at 14:04

    For documentation look at STM32F10xxx_ProgrammingManual.

    Fastest way should be:

    LDRD r1, r2, [r0]

    or

    LDMIA r0, {r1,r2}

    In both ways r1 is loaded with [r0] and r2 with [r0, 4]; r0 is unchanged.

    You can change the ''index'' in many ways (pre, post, up, down) in the same instruction as the load itself.

    If you have a loop, you can read i.e. 8 values in one command and increment r0 to the next unread value:

    LDMIA r0!, {r1-r8}

    LDMIA has better performance in STM32 because the mcu doesn't have a real pipeline infrastructure (the pipeline is blocked in many commands). This command is one of the exceptions that uses the pipeline in fact.

    Tesla DeLorean
    Guru
    May 17, 2011 12:04 PM UTC
    Posted on May 17, 2011 at 14:04

    The LOAD/STORE class instructions typically act on memory, long immediate values are usually loaded from a ''literal pool'' in memory. For register to register (CPU) stuff the MOVE class instructions would be more appropriate, but with 3 operand instructions one usually performs some operation on the register as it's being moved to more effectively use the processor.

    To step through the array, consider

      LDR R0,[R1,#0]

      ADDS R1, R1, #4 ; ADDS R1,#4

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..