ARP requests not transmitted on STM32H735 with FreeRTOS and LWIP
Hello all,
I've spent several days trying to ping my STM32H735 discovery kit with FreeRTOS and LWIP, to no avail.
I've followed this tutorial as a starting point: https://community.st.com/t5/stm32-mcus/how-to-create-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308
I've also investigated on most of the issues mentioned here, without success: https://community.st.com/t5/embedded-software-mcus/how-to-make-ethernet-and-lwip-working-on-stm32/m-p/261456/thread-id/17638
After enabling logs and doing some debugging, I've confirmed that my board successfully receive the ARP request from my computer, etharp_raw sends a raw ARP packet and ethernet_output send a packet. All functions returns a success error code (i.e., 0), so everything is working fine according to the board, but I don't see any outcoming packet on Wireshark.
There is an errata for the STM32H72xx/73xx series, indicating that the ARP offload is not working:
ARP offload function not effective
Description
When the Target Protocol Address of a received ARP request packet matches the device IP address set in the
ETH_MACARPAR register, the source MAC address in the SHA field of the ARP request packet is compared with
the device MAC address in ETH_MACA0LR and ETH_MACA0HR registers (Address0), to filter out ARP packets
that are looping back.
Instead, a byte-swapped comparison is performed by the device. As a consequence, the packet is forwarded to
the application as a normal packet with no ARP indication in the packet status, and the device does not generate
an ARP response.
For example, with the Address0 set to 0x665544332211:
• If the SHA field of the received ARP packet is 0x665544332211, the ARP response is generated while it
should not.
• If the SHA field of the received ARP packet is 0x112233445566, the ARP response not is generated while it
should.
Workaround
Parse the received frame by software and send the ARP response if the source MAC address matches the
byte-swapped Address0.But I'm not sure if that applies to my issue as the logs seems to indicate that the board sent the ARP response, even though it is not the case in the end. I also don't know how to and where the workaround should be applied.
Does someone have any idea on why the ARP response isn't transmitted, even though no error is thrown? Any hints on what I could try?
Thanks a lot for your help and advice!
Regards,
T