Question
ARM DSP with STM32f334c8
Posted on November 11, 2015 at 12:20
Hello ;
I have a problem for the last few days it made be puzzled hope you could help me please . I am using keil compiler with STM32f334c8 ; I had a project based on stm32f429 using FFT from ARM DSP library ; there is a file arm_common_tables.c generate a code size of about 38kbye ; when I move to a new project based on STM32f334c8 the generated code is 160kbyte ! What I am missing here , any I dea please ?arm_status status;
float32_t maxValue;
arm_cfft_radix4_instance_f32 S;
//status = ARM_MATH_SUCCESS;
/* Initialize the CFFT/CIFFT module */
status = arm_cfft_radix4_init_f32(&S, fftSize,
ifftFlag, doBitReverse);
/* Process the data through the CFFT/CIFFT module */
arm_cfft_radix4_f32(&S, testInput_f32_10khz);
/* Process the data through the Complex Magnitude Module for
calculating the magnitude at each bin */
arm_cmplx_mag_f32(testInput_f32_10khz, testOutput,
fftSize);
/* Calculates maxValue and returns corresponding BIN value */
arm_max_f32(testOutput, fftSize, &maxValue, &testIndex);
I am using these code in too diffirent project ; but I get RO size diffirent .
Thank you inadvanced