Skip to main content
SMola
Associate II
September 12, 2018
Question

ARM Cortex M4 SVC interrupt causes usage fault

  • September 12, 2018
  • 6 replies
  • 2246 views

I’m trying to write a context switch assembly on STM32F411E but I encounter a usageFault right after I make a second call to the SVC 0 (in my second task) instruction. The funny thing is the first task can make SVC calls just fine but the second task has issues. The logic for the first and second task is the same so not sure what's causing it. I'm thinking maybe my stack management is bad and so the stack becomes corrupted? I have no way or technique for verifying this hypothesis. I have no way of knowing what I am looking at when I do a stack dump, after the fault occurs.

Here are some of the status register values inside the UsageFault handler, after I make a call to SVC 0, in my second task:

CCR = 0x00000218 
 
HFSR = 0x40000000 
 
CFSR = 0x00000000 
 
DFSR = 0x0000000b 
 
BFSR = 0x00000000
 
BFAR = 0xe000ed38 
 
AFSR = 0x00000000 
 
MMFSR = 0x00000000 
 
MMFAR = 0xe000ed34

Looks like DFSR might provide the biggest clue but I am still not sure what is causing this fault. Has anyone encountered a similar error and can anyone assist me with finding the source of this fault? Why would first call to SVC 0 (in task1) work but the second call to SVC 0 (in task2) fail? It's a bit confusing when CFSR is not telling me what the exact cause of the error because it just reads all zero (CFSR = 0x00000000 ) .

Here’s my context switch code:

/*************************************************** 
 
* activate 
 
* 
 
* Description: context switch routine for tasks 
 
* 
 
* Input: 
 
* 
 
* Output: 
 
* 
 
* Return: 
 
* 
 
* Note: 
 
* 
 
* 
 
***************************************************/ 
 
activate:
 
cpsie i
 
mrs ip, psr 
 
push {r4, r5, r6, r7, r8, r9, r10, r11, ip, lr}
 
ldmfd r0!, {r4, r5, r6, r7, r8, r9, r10, r11, ip, lr}
 
msr control, ip 
 
isb 
 
msr psp, r0
 
/* jump to user task*/ 
 
bx lr
 
 
 
/*************************************************** 
 
* SVC_Handler 
 
* 
 
* Description: 
 
* 
 
* Input: 
 
* 
 
* Output: 
 
* 
 
* Return: 
 
* 
 
* Note: supervisor call (handler mode) 
 
* 
 
* 
 
***************************************************/ 
 
.thumb_func 
 
SVC_Handler:
 
mrs r0, psp 
 
stmdb r0!, {r4, r5, r6, r7, r8, r9, r10, r11, ip, lr}
 
/* load kernel state */ 
 
pop {r4, r5, r6, r7, r8, r9, r10, r11, ip, lr} 
 
msr psr_nzcvq, ip
 
/* back to the thread mode if no other active exception */ 
 
bx lr

If I can even get some tips about how I can debug this (ie. any useful status registers or techniques ?) that would be appreciated. At this point I don't have enough information about the cause so maybe there is someone out there who understands ARM architecture better than me? I'm relatively new to ARM arch to be honest.

This topic has been closed for replies.

6 replies

SMola
SMolaAuthor
Associate II
September 17, 2018

bump

Jeroen3
Senior
September 17, 2018

What is on 0xe000ed38 ?

SMola
SMolaAuthor
Associate II
September 19, 2018

@Community member​ I'm thinking the default value of BFAR register is 0xE000ED38 since the BFSR bits of CFSR register is all zero (BFSR = 0x00000000). In other words, I think the value at that register address (0xe000ed38) is irrelevant since the CFSR is reading zero for all its bit fields.

What do you think?

Jeroen3
Senior
September 19, 2018

"The BusFault Address Register contains the address of the location that generated a BusFault. See the register summary in Table 4.12 for its attributes."

http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0553a/Cihbhdbc.html

SMola
SMolaAuthor
Associate II
September 20, 2018

@Community member​ 

Table 4.30. BFAR bit assignments

Bits Name Function

[31:0] ADDRESS "When the BFARVALID bit of the BFSR is set to 1, this field holds the address of the location that generated the BusFault"

SMola
SMolaAuthor
Associate II
September 20, 2018

The BFARVALID bit of the BFSR is set to zero so the given address shown by "BFAR" is not a valid address.