Skip to main content
Luis Ber
Associate II
Apr 1, 2019 10:51 AM UTC
Solved

Are the VSS and AVSS pins internally connected?

Hello community,

I have a little doubt. Are all the GND pins internally connected inside the microcontroller? Is the analog reference (AVSS) internally connected with the digital one (VSS)? If it not, how is the isolation between them?

I don't know where I can do the union between the analog AGND plane and the digital GND plane and I was thinking if I can use the microcontroller to perform internally the connection.

Thank you in advance!

Luis

This topic has been closed for replies.
Danish1
Danish1Best answer
Lead III
Apr 1, 2019 11:44 AM UTC

One potential confusion: AVss is the negative rail for the analog parts, but it is not always the negative reference for e.g. ADC conversions. It might be for low-pin-count parts, but higher-pin-count parts have VRef- and VssA brought out separately.

I had a look at one data sheet, and the absolute-max ratings state that the voltage between any of the Vss, VssA and VRef- must not exceed 50 mV. So there might be an internal connection.

But I would not want to rely on internal connections to carry any current. I think you are better off making the connection externally. If you are worried about earth loops, why not place the junction between the AGND plane and digital-GND plane beneath the microcontroller.

Hope this helps,

Danish

2 replies

Danish1
Danish1Best answer
Lead III
Apr 1, 2019 11:44 AM UTC

One potential confusion: AVss is the negative rail for the analog parts, but it is not always the negative reference for e.g. ADC conversions. It might be for low-pin-count parts, but higher-pin-count parts have VRef- and VssA brought out separately.

I had a look at one data sheet, and the absolute-max ratings state that the voltage between any of the Vss, VssA and VRef- must not exceed 50 mV. So there might be an internal connection.

But I would not want to rely on internal connections to carry any current. I think you are better off making the connection externally. If you are worried about earth loops, why not place the junction between the AGND plane and digital-GND plane beneath the microcontroller.

Hope this helps,

Danish

Luis Ber
Luis BerAuthor
Associate II
Apr 2, 2019 4:42 PM UTC

Thank you very much Danish.

Finally, I have placed the juntion between the two planes beneath the microcontroller.

Luis