Skip to main content
wb0gaz
Associate III
January 10, 2024
Solved

Application with two STM-32 MCU and one STLINK-V2 port (to one of the MCUs) - cascading possible?

An application will use two STM-32 MCUs - for purpose of this posting, I'll call them "outer" (it's SWDIO and SWCLK pins can be attached to a STLINK-V2 device for firmware downloading), and "inner" (it's SWDIO and SWCLK pins would be tied to two GPIO pins of "outer", and not be externally accessible.)

My question is this - is it possible (by a combination of firmware running on "outer" and appropriate settings to STLINK-V2 such as an acceptable clock frequency) to have the "outer" MCU provide a transparent path (using as-yet undefined firmware running on "outer") so that STLINK-V2 attached to outer's SWDIO/SWCLK pins is passed bit-for-bit to the two GPIO pins (on "outer") which would be connected to SWDIO/SWCLK of "inner" MCU?

The intent of this is to avoid having two separate connectors to which STLINK-V2 would be attached for debug and firmware delivery, and not be reliant on a bootloader (that is, the "inner" processor could be reloaded from scratch using STLINK-V2.)

Happy to answer any request for clarification and be guided in different direction if need be.

Thanks

This topic has been closed for replies.
TDK
TDKBest answer
January 10, 2024

On newer families the hardware capability exists, although I don't think the st-link firmware supports it yet.

On the F0 series, definitely not.

https://community.st.com/t5/stm32-mcus-boards-and-hardware/swd-multidrop-does-any-stm32-or-st-link-support-it/td-p/80861

https://community.st.com/t5/stm32-mcus-products/swd-multi-drop-support-on-stm32l4/m-p/80394

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
January 10, 2024

On newer families the hardware capability exists, although I don't think the st-link firmware supports it yet.

On the F0 series, definitely not.

https://community.st.com/t5/stm32-mcus-boards-and-hardware/swd-multidrop-does-any-stm32-or-st-link-support-it/td-p/80861

https://community.st.com/t5/stm32-mcus-products/swd-multi-drop-support-on-stm32l4/m-p/80394

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
wb0gaz
wb0gazAuthor
Associate III
January 29, 2024

Thanks so much for the pointers!