Skip to main content
ykn
Associate III
November 11, 2022
Question

application code stucked when OTA used on freertos

  • November 11, 2022
  • 0 replies
  • 561 views

hi there,

I am using OTA in freertos, when I used it on bare controller it work properly but As I shifted to freertos, Application code stuck. i search on google, this is beacuse of interrupt.

so I disable all interrupt, Then reset handler executed and jump application code.

but it stuck at particular point . Why this ?

My Reset handler

static void goto_application(void)
{
 printf("Gonna Jump to Application\r\n");
 
 void (*app_reset_handler)(void) = (void*)(*((volatile uint32_t*) (0x08100000 + 4U)));
 
 //__set_MSP(*(volatile uint32_t*) ETX_APP_FLASH_ADDR);
 
 // Turn OFF the Green Led to tell the user that Bootloader is not running
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET ); //Green LED OFF
 app_reset_handler(); //call the app reset handler
}

Thanking you

    This topic has been closed for replies.