Skip to main content
SMein.1
Associate II
Jun 5, 2021 6:09 PM UTC
Question

Any option to go with STM32H745ZIT3 in VOS0 and VOS1 mode to use the maximum clock frequency in the industrial temperature Range variant.

Due to the current semiconductor shortage the microcontroller STM32H745ZIT6 is not available in the quantity of 210, so I had to buy the variant with higher temperature range. However, the data sheet says in small print that this variant does not support VOS0 and VOS1 operation, but I need this mode because otherwise I do not get the computing performance that I need. Is there a way to bypass this lock - it's ok if it makes the temperature higher, I don't need the high temperature range.

This topic has been closed for replies.

2 replies

TDK
Jun 5, 2021 9:57 PM UTC

It's probably one of those things where the performance over the entire temperature range is just not guaranteed. It would be weird for them to disable it in the hardware, but I suppose it's possible.

"If you feel a post has answered your question, please click ""Accept as Solution""."
SMein.1
SMein.1Author
Associate II
Dec 5, 2021 8:35 PM UTC

I tried it and @TDK​  you are answer is correct, it works without problems with 480MHz!! Thanks!