Skip to main content
ASSAAD.ASSAAD
Associate III
March 6, 2014
Question

Analog watchdog/STM32F4

  • March 6, 2014
  • 1 reply
  • 606 views
Posted on March 06, 2014 at 09:37

Hi

I still could not understand the operation of the analog watchdog.

For example I want to protect a short ciruit in the H-bridge ; so I put the shunt resistor and set the limit of the maximum current ; for example if my maximum current is 10A and my shunt resistor is 0.1 ohm ;  the voltage on ADC is 1 V ; for 12 bits ( 3.3 ref) =1241 .

so if I set the high thr of the analog to 1241 ; when adc result equal or great that 1241 it will generate an interrupt .

Is that right ?

Thank you
    This topic has been closed for replies.

    1 reply

    chen
    Associate II
    March 6, 2014
    Posted on March 06, 2014 at 16:46

    Hi

    Based on the description in the reference manual, the ADC analogue watchdog allows you to set threshold values for the ADC value.

    The upper value triggers on a value going above.

    The lower value triggers on a value going below.

    Both can generate an IRQ.

    From your description - the circuit you use must be designed very carefully!

    The ADC input can only withstand a maximum of supply voltage.

    Is your shunt High side ( from supply voltage to bridge)

    Or shunt Low Side ( Bridge to ground)?

    I have worked with the STM32F3 in a switching circuits before. We killed many of them due to spikes on the port pins!

    Heavily protect the ADC inputs. Also if you are driving the H bridge from the STM32 - try protecting the IO pins as well.