Skip to main content
tescaflown
Associate III
June 11, 2015
Question

Analog input ADC, STM32F103, newbie question

  • June 11, 2015
  • 4 replies
  • 1515 views
Posted on June 11, 2015 at 02:00

hello,

I'm discovering how the analog works input in STM32F103. There is something I still didn't find in the datasheet.

I understood all the mode and register configuration, but where is the information to know with wich port is linked to wich ADCx?

For exemple, I need to fullfil the ADCx->SQRx with each number channel I want convert. But where can I find the information that ADCx_INx is Portx?

Is ADC1 is ¨PORTA and ADC2 is PORTB?

Thanks,

    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    June 11, 2015
    Posted on June 11, 2015 at 02:36

    In the datasheet you look for things like ADC123_IN8 or ADC3_IN9, I made those up, the ADC digits would refer to which units they work on, INx is the channel#

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    tescaflown
    Associate III
    June 11, 2015
    Posted on June 11, 2015 at 03:25

    hello,

    I'm sorry but I do not understand you.

    I have the STM32F103 LQFP64 pins. So I have ADC1 and ADC2 and physically, I have pins PAx, PBx (x=0-15)

    You said ''the ADC digits would refer to which units they work on, INx is the channel#''

    I'm ok about that, but for example IN3 is which physically pin (and which ADC)?

    or with another words, when I configure :

    GPIOA->CRL to have PA0 as analog input, how I know which ADCx and which INx channel is?

    I miss something easy and surely trivial but that's what I don't understand.

    Can you help me to make clear my mind?

    Thanks

    tescaflown
    Associate III
    June 11, 2015
    Posted on June 11, 2015 at 06:46

    I finnaly got it. It's in device datasheet, there is alternative name on some pin where we can find the ADCxINx pin.

    I knew that it was silly question, sorry.

    Chris1
    Associate II
    June 11, 2015
    Posted on June 11, 2015 at 15:07

    Incidentally, ''ADC123_INx'' means that a pin can be connected to any of the the three ADCs, ADC12_INx means that the pin can connect to ADC1 and / or ADC2, but not ADC3.  Similarly, ADC3_INx connects only to ADC3.