Skip to main content
Associate II
Nov 24, 2023 3:11 PM UTC
Solved

AN5290 Possible Typo in LDO configuration for VDD > 2.5 V Section

AN5290 discusses a workaround for the "When VDD exceeds 2.5V in LDO configuration a glitch on HSE may create a hard fault on M4/M0" issue identified in the errata. In the AN5290 section titled "1.2 LDO configuration for VDD > 2.5 V"  recommends:

The recommended values (see Figure 3) are:
• Inductance: 1.8 ± 0.1 nH, 6 GHz ± 15% self-resonance frequency, 1000 mA rated
current (for example, Murata LQG15HS1N8B02)
• Resistor: 2.2 Ω, able to support 1 W for 5 ns (for example, Vishay D10/CRCW0402e3)

However in Figure 3 it shows a 1.2nH inductor.

Not sure if this is the correct form to identify these discrepancies, so if someone could let me know the best location for these issues that would be great. 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Nov 24, 2023 5:19 PM UTC

Hi again @alexRossRBR 

Thank you for having reported this issue.

An internal ticket (number: 167173) is submitted to escalate this issue internally for check and analysis.
(PS: number 167173 is an internal tracking number and not available outside of ST).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STTwo-32
ST Technical Moderator
Nov 24, 2023 3:13 PM UTC

Hello @alexRossRBR 

thank you for your request.  I will check this internally and come back to you as soon as possible.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Nov 24, 2023 5:19 PM UTC

Hi again @alexRossRBR 

Thank you for having reported this issue.

An internal ticket (number: 167173) is submitted to escalate this issue internally for check and analysis.
(PS: number 167173 is an internal tracking number and not available outside of ST).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.