An STM tutorial on timers has errors regarding PWM mode, for STM32 MCUs
An STM tutorial on timers has errors regarding PWM mode, for STM32.
The tutorial is: "STM32L4 - Timers : Advanced-control, general-purpose, and basic timers"
It is a slide-set, with notes. There are at least a couple versions of it, e.g., a version for STM32WB.
https://www.st.com/resource/en/product_training/STM32L4_WDG_TIMERS_GPTIM.pdf
The tutorial's introduction indicates the slides are describing STM32 timers in general. This is corroborated by the reference manuals for STM32L4 and STM32F76xxx [STM18, STM20]. The manuals have identical sections titled "PWM mode".
#### Problem Summary ####
The problems are summarized here, and more info is in the "Details" section, below.
References are listed at the end.
#### The duty-cycle equations are incorrect:
In the tutorial, on page 32, this equation appears to be incorrect:
duty_cycle = (CCRx + 1)/(ARR + 1)
I think it should be:
duty_cycle = CCRx/(ARR + 1)
The STM32L4 reference-manual describes how CCRx specifies the duty-cycle [STM18, pages 938f]. It does not seem to involve adding 1 to CCRx.
Similarly, on the tutorial's page 32, the derived equation is incorrect:
CCRx = (duty_cycle * (ARR+1)) - 1
To illustrate the error, a duty-cycle of 0 results in a CCRx value of -1, which can't be stored in CCRx.
#### The PWM-resolution equations are incorrect
In the tutorial, on page 32, this equation appears to be incorrect:
Res(steps) = Ftim / Fpwm
The problem is that those frequencies are based on different units, so they can't be divided in a meaningful way.
* Ftim is the clock frequency, i.e., clock_tics/second
* Fpwm is based on a scaled-clock frequency, i.e., scaled_clock_tics/second
The equation for Fpwm is given earlier, on page 31. PSC is the prescaler register:
Fpwm = Ftim / ((ARR + 1) * (PSC + 1))
Resolving the Res(steps) equation leads to:
Res(steps) = (ARR+1) * (PSC+1)
This is the number of clock-tics per PWM cycle. That doesn't make sense as the PWM resolution, unless PSC is 0.
#### Problem Details ####
#### The duty-cycle equations are incorrect:
In the tutorial, on page 32, this equation appears to be incorrect:
duty_cycle = (CCRx + 1)/(ARR + 1)
I think it should be:
duty_cycle = CCRx/(ARR + 1)
For example, the STM32L4 reference-manual specifies the following for PWM mode 1, in edge-aligned mode with up-counting [STM18, page 939]:
* CCRx specifies how long the signal is high. So, (CCRx+1) does not specify how long the signal is high, as the tutorial seems to claim.
* (ARR+1) specifies how long the PWM cycle is.
* For CCRx and ARR, the units are in scaled-clock-tics (scaled by (PSC+1))
* A CCRx value of 0 specifies a duty-cycle of 0.
* A CCRx value greater-than ARR specifies a duty-cycle of 100%
That errant equation does not allow for a duty_cycle of 0. Setting CCRx to 0 does not produce a duty_cycle of 0.
Also, the errant equation calculates a duty-cycle greater than 100% for a CCRx value greater-than the ARR value.
Similarly, on the tutorial's page 32, the derived equation is incorrect:
CCRx = (duty_cycle * (ARR+1)) - 1
There, a duty_cycle of 0 calculates a CCRx value of -1, which isn't possible.
Also, a duty_cycle of 100% does not calculate a CCRx value greater than the ARR value, which is required.
#### The PWM resolution equations are incorrect
In the tutorial, on page 32, this equation appears to be incorrect:
Res(steps) = Ftim / Fpwm
The problem is that these frequencies are based on different units, so they can't be divided in a meaningful way.
Ftim is the clock frequency, i.e., clock_tics/second
Fpwm is based on a scaled-clock frequency (scaled by (PSC+1)), i.e., the units are scaled_clock_tics/second.
The equation for Fpwm is on page 31:
Fpwm = Ftim / ((ARR + 1) * (PSC + 1))
Resolving the Res(steps) equation leads to:
Res(steps) = (ARR+1) * (PSC+1)
This is the number of clock-tics per PWM cycle, which doesn't make sense as the PWM resolution.
For example, if ARR is 0, there's minimal PWM resolution. There are only two possible duty-cycles: 0% and 100%. Increasing PSC will not increase the duty-cycle resolution. However, in the equation, increasing PSC would increase the resolution, for an ARR of 0.
The Res(steps) equation is only correct when PSC is zero.
For example, there is an STM Applicaton Note on PWM resolution, and it uses the same Res(steps) equation as the tutorial [STM17, page 6]. However, the STM Applicaton Note makes no mention of a prescaler being used.
In the tutorial, page 32 also has a derived equation using log base-2. So, it's also incorrect.
#### References ####
[STM17] STM, "PWM resolution enhancement through a dithering technique for STM32 advanced-configuration, general-purpose and lite timers", Application note AN4507, January 2017
[STM18] STM, "Reference manual : STM32F76xxx and STM32F77xxx advanced Arm-based 32-bit MCUs", RM0410, March 2018
[STM21] STM, "STM32L47xxx, STM32L48xxx, STM32L49xxx and STM32L4Axxx advanced Arm-based 32-bit MCUs", Reference manual RM0351, June 2021