Question
Alternative to NSS?
Posted on June 23, 2015 at 00:34
Hi. I've never designed with STM before and I have to admit I've not fully studied the datasheets. We're in prelim design phase right now. I tentatively have the pins for an STM32F205 fully specified, and I realize now we have what appears to be a problem. We require both DACs, one of which is on PA4. This pin is also used for SPI1_NSS and SPI3_NSS. SPI1_NSS and SPI3_NSS can also be on PA15. That's fine if we need only SPI1
or
SPI3... But we need all 3 SPI and both DAC.Is there a way to use a different GPIO or the NSS function? Or I'm stuck either using an external DAC or finding a different chip? I don't have any spare gpio, but we can move up to the 100pin version of the chip if necessary... but that still has the same ''problem'' wrt DAC/NSS.Thank you.