Skip to main content
arunl4g
Associate III
February 18, 2016
Question

Alternative Function

  • February 18, 2016
  • 1 reply
  • 476 views
Posted on February 18, 2016 at 09:48

Hi 

i wonder if it is possible to read the changes on the GPIO pin where the GPIO pin is configured as GPIO_Mode  = AF pin mode.  on f429?
    This topic has been closed for replies.

    1 reply

    waclawek.jan
    Super User
    February 18, 2016
    Posted on February 18, 2016 at 10:50

    Yes.

    See last point in 8.3.11 Alternate function configuration, in RM0090 rev.11.

    JW