Skip to main content
迪嘉拉.1
Visitor II
June 17, 2021
Question

ALL HI�? I am currently using the RTC function of STM32F103, the external passive 32.768KHz crystal and 20p matching capacitor.

  • June 17, 2021
  • 1 reply
  • 596 views

ALL HI�?

I am currently using the RTC function of STM32F103, the external passive 32.768KHz crystal and 20p matching capacitor.The RTC function is configured on the software program, and the RTC has been started. But I can't see 32.768KHz waveform when I use oscilloscope to measure the output pin of external crystal. Please confirm the reason. Or provide specific measurement methods or pictures. Thank you.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
June 17, 2021

Probing the pins directly interferes with the loading, on the F1 doesn't the RTC have the ability to output via the TAMPER pin? Check the Data Sheet and Reference Manual

The clock does not start automatically. You should look for PWR or RTC examples provided by CubeF1 packages

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..