Skip to main content
Prashant Chopade
Associate
July 14, 2018
Question

After converting LwIP_HTTP_Server_Netconn_RTOS to C++, hangs in Hal_Delay()

  • July 14, 2018
  • 1 reply
  • 563 views
Posted on July 14, 2018 at 12:20

Hi,

I was working with LwIP_HTTP_Server_Netconn_RTOS on STM32F469I-Eval board.

I converted main.c, httpser-netconn.c to main.cpp and httpser-netconn.cpp

Was able to compile it successfully, but when I did debug, it hanged at ethernetif_init()->low_level_init()->HAL_ETH_Init() -> HAL_Delay() forever.

Even 'uwTick' from HAL_GetTick() had increased till 16 only and that count stopped there forever.

Will help me great if I get some help on how to proceed ahead? or some pin-points to resolve it out?

Regards,

Prashant

    This topic has been closed for replies.

    1 reply

    Prashant Chopade
    Associate
    July 14, 2018
    Posted on July 14, 2018 at 15:02

    My modified main() is:

    int main(void)

    {

    /* STM32F4xx HAL library initialization:

    - Configure the Flash prefetch, instruction and Data caches

    - Configure the Systick to generate an interrupt each 1 msec

    - Set NVIC Group Priority to 4

    - Global MSP (MCU Support Package) initialization

    */

    HAL_Init();

    /* Configure the system clock to 180 MHz */

    SystemClock_Config();

    /* Init thread */

    #if defined(__GNUC__)

    // osThreadDef(Start, StartThread, osPriorityNormal, 0, configMINIMAL_STACK_SIZE * 5);

    #else

    osThreadDef(Start, StartThread, osPriorityNormal, 0, configMINIMAL_STACK_SIZE * 2);

    #endif

    // osThreadCreate (osThread(Start), NULL);

    BSP_Config();

    /* Create tcp_ip stack thread */

    tcpip_init(NULL, NULL);

    /* Initialize the LwIP stack */

    Netif_Config();

    http_server_netconn_init();

    User_notification(&gnetif);

    /* Start scheduler */

    osKernelStart();

    /* We should never get here as control is now taken by the scheduler */

    for( ;; );

    }