Advanced-control timers (TIM1&TIM8) Center-aligned mode (up/down counting)
Evaluating the STM32F207 for a project.
I need to create a triangle waveform, starting from an arbitrary point between two limits, and it needs to be able to start in both incrementing or decrementing fashion. I intend to use DMA to play this waveform out to a DAC
I am looking at Advanced-control timers (TIM1&TIM8) Center-aligned mode (up/down counting), I understand that this only works between 0 and TIMx_ARR but I can offset the waveform to the correct point
From the manual page 297 I understand that
“In center-aligned mode, the counter counts from 0 to the auto-reload value (content of the TIMx_ARR register) – 1�
and that
“In this mode, the DIR direction bit in the TIMx_CR1 register cannot be written. It is updated
by hardware and gives the current direction of the counter.�
This indicates to me that when the mode is set the Counter register (TIMx_CNT) is cleared and the DIR direction bit is set to increment.
Question
1>Can the Counter register (TIMx_CNT) be loaded to an arbitrary value after the mode is set if the waveform needs to increment
2>If the waveform needs to start decrementing, could the TIMx_ARR register be set to a small value the timer run until the the limit is hit (now in the right state). Timer disabled (Bit 0 CEN: Counter enable). Then the TIMx_ARR and the Counter register (TIMx_CNT) register set to the proper value, and then reenabled
Thanks in advance
Joe
From the manual
******************************************
Advanced-control timers (TIM1&TIM8)
Page 297
Center-aligned mode (up/down counting)
In center-aligned mode, the counter counts from 0 to the auto-reload value (content of the
TIMx_ARR register) – 1, generates a counter overflow event, then counts from the autoreload
value down to 1 and generates a counter underflow event. Then it restarts counting
from 0.
In this mode, the DIR direction bit in the TIMx_CR1 register cannot be written. It is updated
by hardware and gives the current direction of the counter.
Page 329
Bits 6:5 CMS[1:0]: Center-aligned mode selection
….
….
11: Center-aligned mode 3. The counter counts up and down alternatively. Output compare
interrupt flags of channels configured in output (CCxS=00 in TIMx_CCMRx register) are set
both when the counter is counting up or down.
Note: It is not allowed to switch from edge-aligned mode to center-aligned mode as long as
the counter is enabled (CEN=1)
Bit 4 DIR: Direction
0: Counter used as upcounter
1: Counter used as downcounter
Note: This bit is read only when the timer is configured in Center-aligned mode or Encoder
mode.
******************************************