Skip to main content
leventeyigel52
Associate III
January 13, 2012
Question

Adress Type (Flash Memory)

  • January 13, 2012
  • 7 replies
  • 1584 views
Posted on January 13, 2012 at 10:23

Hi,

I want to read all the datas of the Flash Memory on STM32F103RB

// Adress start value = 0x08000000 ,end value = 0x0801FFFF;

while(Adress != 0x0801FFF) {

 FLASH_Unlock();             

 Data=*((uint16_t *) Adres);  //read at 0x08000000 flash memory address 

        FLASH_Lock(); 

        Adres=Adres+2;

        USART_SendData(USART2,Data); 

}

When this program runs, Adress data turns decimal type and i can't see the values .

What can i do for describing Adress's data type to increasing hexadecimal type ?

    This topic has been closed for replies.

    7 replies

    rosarium
    Associate
    January 13, 2012
    Posted on January 13, 2012 at 12:06

    In the linker script:

    MEMORY

    {

      

    RAM_C (xrw) : ORIGIN = 0x10000000, LENGTH = 64K

      

    RAM_D (xrw) : ORIGIN = 0x20000000, LENGTH = 128K

      

    FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K

    }

    leventeyigel52
    Associate III
    January 13, 2012
    Posted on January 13, 2012 at 12:21

    I tried to say how can i define the adress value and increase it. 

    I have a for loop and the adress value is increase in the loop, thus i can get the values on all of the adresses in flash memory ?

    When i define ''u32 Adress=0x08000000;'' or ''uint32_t Adress'' or ''uint64_t Adress;'' this returns me decimal values and i dont want this,i want to debug with hexadecimal form.

     Can you read the source code  and give me advice about this ? 

    leventeyigel52
    Associate III
    January 13, 2012
    Posted on January 13, 2012 at 12:24

    for(i=0;i<65536;i++) {

            FLASH_Unlock();             

            Data=*((uint16_t *) Adress); //read at Adress^s value flash memory address 

            FLASH_Lock(); 

            Adress=Adress+2;

            USART_SendData(USART2,Data); 

            }

    I have the problem at this loop and Adress increasing problem.

    Tesla DeLorean
    Guru
    January 13, 2012
    Posted on January 13, 2012 at 12:32

    a) You don't need to Lock/Unlock the flash memory to read it

    b) USART_SendData is not going to consume 16-bit words c) You need to check the TXE status of the USART before sending each byte d) Your terminal address is wrong

    // Address start value = 0x08000000 ,end value = 0x0801FFFF;
    uint16_t Data;
    uint32_t Address;
    Address = 0x08000000;
    while(Address < 0x0801FFFF) // 512KB limit
    {
    Data= *((uint16_t *)Address); //read at 0x08000000+ flash memory address 
    Address += 2;
    while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
    USART_SendData(USART2,((Data >> 0) & 0xFF)); // Send Low Byte
    while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
    USART_SendData(USART2,((Data >> 8) & 0xFF)); // Send High Byte
    }

    This will send the data as raw 8-bit bytes. Plus it will probably overflow the console, and get some corruption. Usually you'd send it in small blocks, with a checksum. Want the data in hex digits, then you're going to need to break the bytes down into ASCII hex/alpha characters. Want pretty formatting, you'll need to add the code to do that.

    void SendHexByte(uint16_t Data)
    {
    static const char Hex[]=''0123456789ABCDEF'';
    while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
    USART_SendData(USART2,(Hex[(Data >> 4) & 0xF)]); // Send High Nibble
    while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
    USART_SendData(USART2,(Hex[(Data >> 0) & 0xF)]); // Send Low Nibble
    }

    void DumpFlash(void)
    {
    uint16_t Data;
    uint32_t Address;
    for(Address = 0x08000000; Address<
    0x08020000
    ; Address += 2)
    {
    Data= *((uint16_t *)Address); //read at 0x08000000+ flash memory address 
    SendHexByte(((Data >> 0) & 0xFF)); // Send Low Byte
    SendHexByte(((Data >> 8) & 0xFF)); // Send High Byte
    }
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    leventeyigel52
    Associate III
    January 13, 2012
    Posted on January 13, 2012 at 13:59

    I solved this problem thanks to you ..

    Thanks clive1 !!!!!

    leventeyigel52
    Associate III
    January 16, 2012
    Posted on January 16, 2012 at 08:51

    clive1

    your code helped me,thanks a lot again . I'll ask you a question again

    I want to see these adresses and datas like ->

    0x08000000  0x07CE

    0x08000002  0xFFFF

    .. ..

    ...

    ...

    0x0801FFFF  0xFFFF

    on  the hyper terminal screen

    Adress value is 32-bit so I can't write the algorithm or code  for this.

    Can u help me about it ?How can we send Adress's value 

    Tesla DeLorean
    Guru
    January 16, 2012
    Posted on January 16, 2012 at 14:46

    void SendChar(char Data)
    {
    while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET);
    USART_SendData(USART2, Data);
    }
    void SendHexByte(uint16_t Data)
    {
    static const char Hex[]=''0123456789ABCDEF'';
    SendChar(Hex[((Data >> 4) & 0xF])); // Send High Nibble
    SendChar(Hex[((Data >> 0) & 0xF)]); // Send Low Nibble
    }
    void SendHexWord(uint16t Data)
    {
    SendHexByte(((Data >> 8) & 0xFF)); // Send High Byte
    SendHexByte(((Data >> 0) & 0xFF)); // Send Low Byte
    }
    void SendHexDword(uint32t Data)
    {
    SendHexWord((uint16_t)((Data >> 16) & 0xFFFF)); // Send High Word
    SendHexWord((uint16_t)((Data >> 0) & 0xFFFF)); // Send Low Word
    }
    void DumpFlash(void)
    {
    uint16_t Data;
    uint32_t Address;
    for(Address = 0x08000000; Address<0x08020000; Address += 2)
    {
    Data= *((uint16_t *)Address); //read at 0x08000000+ flash memory address
    SendChar('0')
    SendChar('x')
    SendHexDword(Address);
    SendChar(' ')
    SendChar('0')
    SendChar('x')
    SendHexWord(Data);
    SendChar('
    ');
    SendChar('
    ');
    }
    }

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..