Skip to main content
khouja_houssem
Associate III
Sep 4, 2013 7:37 PM UTC
Question

Adding RAM to STM32F4

Posted on September 04, 2013 at 21:37

Hi,

For my project I need additional RAM, is it possible to add memory to the STM32F407VG (in the STM32F4-Discovery Board) using the FSMC interface?

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    Sep 4, 2013 7:58 PM UTC
    Posted on September 04, 2013 at 21:58

    Review schematics and pin allocations for boards using external memory, like STM3240G-EVAL or RedDragon407

    Look also for daughter boards which you can plug the STM32F4-Discovery into.

    Personally I'd be looking for a different board, with a higher pin count STM32 part to better accommodate the DCMI and FSMC interfaces. Check eBay, etc.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    khouja_houssem
    Associate III
    Sep 4, 2013 8:19 PM UTC
    Posted on September 04, 2013 at 22:19

    Thanks for your answer CLIVE1.

    In the STM32F4-Eval board we have only 8 address outputs (A16 to A23). 

    What can be the maximum memory they could controle? Can it reach 16MB?
    Tesla DeLorean
    Guru
    Sep 4, 2013 9:24 PM UTC
    Posted on September 04, 2013 at 23:24

    About 256 or 512 bytes depending on if your data bus is 8 or 16-bit wide?

    I haven't looked at the STM32F4-Discovery being a practical platform for external memory, depending on the memory you'd have to wire up ~30 pins. The camera would be another ~20 pins

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..