Question
Add CubeMX support for dual buffer DMA in ADC modes.
This is a suggestion, not a question...
There's no support for dual buffer DMA mode in the ADC HAL, and it would be very easily added.
Already did my own copying the existing function for the multimodeDMA.
The problem is that CubeMX will wipe the code after each code generation.
/**
* @brief Enables ADC DMA request after last transfer (Multi-ADC mode) and enables ADC peripheral
* Configures the DMA in double buffer mode
*
* @note Caution: This function must be used only with the ADC master.
* DMA must be configured in Circular buffer mode
*
* @param hadc pointer to a ADC_HandleTypeDef structure that contains
* the configuration information for the specified ADC.
* @param FirstMemAddress Pointer to the first buffer in which transferred from ADC peripheral to memory will be stored.
* @param SecondMemAddress Pointer to the second buffer in which transferred from ADC peripheral to memory will be stored.
* @param Length The length of data to be transferred from ADC peripheral to memory.
* @retval HAL status
*/
HAL_StatusTypeDef HAL_ADCEx_MultiModeStart_DualBF_DMA(ADC_HandleTypeDef* hadc, uint32_t *FirstMemAddress, uint32_t *SecondMemAddress, uint32_t DataLength)
{
__IO uint32_t counter = 0U;
ADC_Common_TypeDef *tmpADC_Common;
/* Check the parameters */
assert_param(IS_FUNCTIONAL_STATE(hadc->Init.ContinuousConvMode));
assert_param(IS_ADC_EXT_TRIG_EDGE(hadc->Init.ExternalTrigConvEdge));
assert_param(IS_FUNCTIONAL_STATE(hadc->Init.DMAContinuousRequests));
/* Process locked */
__HAL_LOCK(hadc);
/* Check if ADC peripheral is disabled in order to enable it and wait during
Tstab time the ADC's stabilization */
if((hadc->Instance->CR2 & ADC_CR2_ADON) != ADC_CR2_ADON)
{
/* Enable the Peripheral */
__HAL_ADC_ENABLE(hadc);
/* Delay for temperature sensor stabilization time */
/* Compute number of CPU cycles to wait for */
counter = (ADC_STAB_DELAY_US * (SystemCoreClock / 1000000U));
while(counter != 0U)
{
counter--;
}
}
/* Start conversion if ADC is effectively enabled */
if(HAL_IS_BIT_SET(hadc->Instance->CR2, ADC_CR2_ADON))
{
/* Set ADC state */
/* - Clear state bitfield related to regular group conversion results */
/* - Set state bitfield related to regular group operation */
ADC_STATE_CLR_SET(hadc->State,
HAL_ADC_STATE_READY | HAL_ADC_STATE_REG_EOC | HAL_ADC_STATE_REG_OVR,
HAL_ADC_STATE_REG_BUSY);
/* If conversions on group regular are also triggering group injected, */
/* update ADC state. */
if (READ_BIT(hadc->Instance->CR1, ADC_CR1_JAUTO) != RESET)
{
ADC_STATE_CLR_SET(hadc->State, HAL_ADC_STATE_INJ_EOC, HAL_ADC_STATE_INJ_BUSY);
}
/* State machine update: Check if an injected conversion is ongoing */
if (HAL_IS_BIT_SET(hadc->State, HAL_ADC_STATE_INJ_BUSY))
{
/* Reset ADC error code fields related to conversions on group regular */
CLEAR_BIT(hadc->ErrorCode, (HAL_ADC_ERROR_OVR | HAL_ADC_ERROR_DMA));
}
else
{
/* Reset ADC all error code fields */
ADC_CLEAR_ERRORCODE(hadc);
}
/* Process unlocked */
/* Unlock before starting ADC conversions: in case of potential */
/* interruption, to let the process to ADC IRQ Handler. */
__HAL_UNLOCK(hadc);
/* Set the DMA transfer complete callback */
hadc->DMA_Handle->XferCpltCallback = ADC_MultiModeDMAConvCplt;
hadc->DMA_Handle->XferM1CpltCallback = ADC_MultiModeDMAConvCplt;
/* Set the DMA half transfer complete callback */
hadc->DMA_Handle->XferHalfCpltCallback = ADC_MultiModeDMAHalfConvCplt;
hadc->DMA_Handle->XferM1HalfCpltCallback = ADC_MultiModeDMAHalfConvCplt;
/* Set the DMA error callback */
hadc->DMA_Handle->XferErrorCallback = ADC_MultiModeDMAError ;
/* Manage ADC and DMA start: ADC overrun interruption, DMA start, ADC */
/* start (in case of SW start): */
/* Clear regular group conversion flag and overrun flag */
/* (To ensure of no unknown state from potential previous ADC operations) */
__HAL_ADC_CLEAR_FLAG(hadc, ADC_FLAG_EOC);
/* Enable ADC overrun interrupt */
__HAL_ADC_ENABLE_IT(hadc, ADC_IT_OVR);
/* Pointer to the common control register to which is belonging hadc */
/* (Depending on STM32F4 product, there may be up to 3 ADC and 1 common */
/* control register) */
tmpADC_Common = ADC_COMMON_REGISTER(hadc);
if (hadc->Init.DMAContinuousRequests != DISABLE)
{
/* Enable the selected ADC DMA request after last transfer */
tmpADC_Common->CCR |= ADC_CCR_DDS;
}
else
{
/* Disable the selected ADC EOC rising on each regular channel conversion */
tmpADC_Common->CCR &= ~ADC_CCR_DDS;
}
/* Enable the DMA Stream */
HAL_DMAEx_MultiBufferStart_IT(hadc->DMA_Handle,(uint32_t)&tmpADC_Common->CDR, (uint32_t) FirstMemAddress, (uint32_t) SecondMemAddress, (uint32_t) DataLength);
/* if no external trigger present enable software conversion of regular channels */
if((hadc->Instance->CR2 & ADC_CR2_EXTEN) == RESET)
{
/* Enable the selected ADC software conversion for regular group */
hadc->Instance->CR2 |= (uint32_t)ADC_CR2_SWSTART;
}
}
/* Return function status */
return HAL_OK;
}