Skip to main content
MDali.1
Associate
Apr 20, 2023 1:30 PM UTC
Solved

ADC3+DMA

I'm having trouble with my STM32h757 processor.

I'm trying to sample 2000 samples using ADC3+DMA1/DMA2/BDMA, but it's not working as expected.

I set up the ADC to work in continuous mode and the DMA to work in circular mode with the address increment set to half-word.

However, when I start the sampling process, the DMA doesn't increment the address and only the first value in the buffer is changing.

I've tried defining the buffer in domain 1, 2, and 3, but it didn't make a difference in the behavior.

IN addition, everything works fine when I use ADC1 instead of ADC3.

Any ideas on what might be causing the issue and how to fix it?

Thanks for your help.

This topic has been closed for replies.
MDali.1
MDali.1Best answer
Associate
Apr 20, 2023 4:15 PM UTC

Hello Romain, 

I have upgraded my IDE from version 1.10.1 to version 1.12.0. After the upgrade, I have tested my code and everything appears to be functioning properly.

Thanks for your assistance.

Meni

3 replies

RomainR.
ST Employee
Apr 20, 2023 2:30 PM UTC

Hello @MDali.1 (Community Member)

If I understand well, you sample only one ADC value in the buffer.

Can you share your ADC3 and DMA (or BDMA) configuration, to try to reproduce your issue ?

Best regards,

Romain

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MDali.1
MDali.1AuthorBest answer
Associate
Apr 20, 2023 4:15 PM UTC

Hello Romain, 

I have upgraded my IDE from version 1.10.1 to version 1.12.0. After the upgrade, I have tested my code and everything appears to be functioning properly.

Thanks for your assistance.

Meni

RomainR.
ST Employee
Apr 21, 2023 6:34 AM UTC

Hello Hello @MDali.1 (Community Member)

Good news, but it shouldn't that be the reason for the problem you were having?

Did you also change something in your codes?

Best regards,

Romain

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.