Question
ADC3 channel 7 in discoveryf4 board
Posted on January 03, 2015 at 13:43
hi
i want to test an example in that explains ADC3 using channel7 with DMA there is Configure ADC Channel7 pin as analog input GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOF, &GPIO_InitStructure); now i can not find GPIOF_pin_9 on the discovery board what should i do now? can i replace it with another pin from another port? #!winning-rtfm